<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What is the correct PCB design impedance to use for an LPC4330 GPIO/SGPIO output pin? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-is-the-correct-PCB-design-impedance-to-use-for-an-LPC4330/m-p/746549#M30106</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tim Hutcheson,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you for your interest in LPC product, I would like to provide service for you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; As I know, the GPIO/SGPIO don't have the specific PCB layout impendance requirement. If the wire length is less than two inches, I think you don't need to add 33-50 ohm.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Actually, we have an application note: &lt;A href="https://www.nxp.com/docs/en/application-note/AN11343.zip" target="_blank"&gt;&lt;STRONG&gt;SGPIO camera module design using LPC4300 &lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp; &lt;/STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can refer to the application note, there has a PCB board which is drawn by eagle design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21349i4A23356E5D620F0D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You can find the SGPIO layout also don't have the resistor. About the wire wide, you also can refer to this board, it is 8mils.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question about it, please kindly let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Mar 2018 06:24:22 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2018-03-29T06:24:22Z</dc:date>
    <item>
      <title>What is the correct PCB design impedance to use for an LPC4330 GPIO/SGPIO output pin?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-is-the-correct-PCB-design-impedance-to-use-for-an-LPC4330/m-p/746548#M30105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In particular, I' designing a high speed SGPIO 8 lane transfer pipe between two LPC4330 and am interested to know if I can avoid adding 33-50 ohm series resistors for a length of less than two inches between processors or not.&lt;/P&gt;&lt;P&gt;I was not able to find any impedance information in the literature available but assume that no source resistors a re built into the device.&amp;nbsp; Is that true?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2018 21:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-is-the-correct-PCB-design-impedance-to-use-for-an-LPC4330/m-p/746548#M30105</guid>
      <dc:creator>timhutcheson</dc:creator>
      <dc:date>2018-03-28T21:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: What is the correct PCB design impedance to use for an LPC4330 GPIO/SGPIO output pin?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-is-the-correct-PCB-design-impedance-to-use-for-an-LPC4330/m-p/746549#M30106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tim Hutcheson,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you for your interest in LPC product, I would like to provide service for you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; As I know, the GPIO/SGPIO don't have the specific PCB layout impendance requirement. If the wire length is less than two inches, I think you don't need to add 33-50 ohm.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Actually, we have an application note: &lt;A href="https://www.nxp.com/docs/en/application-note/AN11343.zip" target="_blank"&gt;&lt;STRONG&gt;SGPIO camera module design using LPC4300 &lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp; &lt;/STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can refer to the application note, there has a PCB board which is drawn by eagle design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21349i4A23356E5D620F0D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You can find the SGPIO layout also don't have the resistor. About the wire wide, you also can refer to this board, it is 8mils.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question about it, please kindly let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2018 06:24:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-is-the-correct-PCB-design-impedance-to-use-for-an-LPC4330/m-p/746549#M30106</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-03-29T06:24:22Z</dc:date>
    </item>
  </channel>
</rss>