<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: fsl_dspi.h file missing</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745766#M30072</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry &lt;/P&gt;&lt;P&gt;I use MCUXpresso IDE v11.2.0_4120 with SDK 2.8.0&lt;/P&gt;&lt;P&gt;but I did not find the fsl_sdspi_disk.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the diskio.c you supported it&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;Nino&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Aug 2020 12:11:58 GMT</pubDate>
    <dc:creator>bahn</dc:creator>
    <dc:date>2020-08-12T12:11:58Z</dc:date>
    <item>
      <title>fsl_dspi.h file missing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745761#M30067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SDK: LPC54628 2.3.0&lt;/P&gt;&lt;P&gt;When I config a new project with this SDK, a head file (fat fs) miss when compiled: fsl_dspi.h. I search sdk directory, no such file.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;../fatfs/fatfs_source/fsl_sdspi_disk.c:39:22: fatal error: fsl_dspi.h: No such file or directory&lt;BR /&gt;&amp;nbsp;#include "fsl_dspi.h"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;anyone can help me? Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jan 2018 03:54:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745761#M30067</guid>
      <dc:creator>lianboli</dc:creator>
      <dc:date>2018-01-23T03:54:38Z</dc:date>
    </item>
    <item>
      <title>Re: fsl_dspi.h file missing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745762#M30068</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a similar problem with using SD card(fat fs) on KL27Z - SDK 2.3.0. I'm also missing &lt;EM&gt;fsl_dspi.h&lt;/EM&gt;. I found that in SDK v. 2.0 &lt;EM&gt;fsl_dspi&amp;nbsp;&lt;/EM&gt; is a driver for SPI and in the 2.3 version this driver is replaced with &lt;EM&gt;fsl_spi.&lt;/EM&gt;&amp;nbsp; I think that in &lt;EM&gt;fsl_sdspi_disk -&amp;nbsp;&lt;/EM&gt;the spi&amp;nbsp;should be configured with the new driver. (rewrite functions spi_init: &lt;EM&gt;dspi_transfer_t = spi_transfer_t&lt;/EM&gt; ,spi_exchange,spi_set_frequency, &lt;SPAN style="color: #333333; background-color: #ffffff;"&gt;etc.&lt;/SPAN&gt;). I didn't have time to implement this changes, so I don't know if it will work.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jan 2018 19:18:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745762#M30068</guid>
      <dc:creator>hudo</dc:creator>
      <dc:date>2018-01-23T19:18:50Z</dc:date>
    </item>
    <item>
      <title>Re: fsl_dspi.h file missing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745763#M30069</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Steven,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working with this issue. Meanwhile if what you need to do is read/write in an SD card you can check the SDK example "sdcard_fatfs" that works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Victor Jimenez.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jan 2018 21:08:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745763#M30069</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-01-29T21:08:18Z</dc:date>
    </item>
    <item>
      <title>Re: fsl_dspi.h file missing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745764#M30070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need fat fs support. So I am waiting for your updated SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Steven&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 03:18:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745764#M30070</guid>
      <dc:creator>lianboli</dc:creator>
      <dc:date>2018-01-30T03:18:31Z</dc:date>
    </item>
    <item>
      <title>Re: fsl_dspi.h file missing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745765#M30071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steven,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This bug&amp;nbsp;was already reported with the developers so it will be fix in future releases of the SDK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Victor Jimenez.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Mar 2018 20:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745765#M30071</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-03-13T20:31:35Z</dc:date>
    </item>
    <item>
      <title>Re: fsl_dspi.h file missing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745766#M30072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry &lt;/P&gt;&lt;P&gt;I use MCUXpresso IDE v11.2.0_4120 with SDK 2.8.0&lt;/P&gt;&lt;P&gt;but I did not find the fsl_sdspi_disk.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the diskio.c you supported it&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;Nino&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2020 12:11:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/fsl-dspi-h-file-missing/m-p/745766#M30072</guid>
      <dc:creator>bahn</dc:creator>
      <dc:date>2020-08-12T12:11:58Z</dc:date>
    </item>
  </channel>
</rss>