<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC546xx USB1 Examples</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-Examples/m-p/743662#M29987</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm&amp;nbsp;developing a bare metal project on a custom board with a LPC54616 and need to get it working as a mass storage device using the USB1 controller.&lt;/P&gt;&lt;P&gt;Does anyone know if there are any LPC546xx&amp;nbsp;example projects which demonstrate using USB1, preferably as a device?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Matt...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Mar 2018 12:09:56 GMT</pubDate>
    <dc:creator>mattskey</dc:creator>
    <dc:date>2018-03-28T12:09:56Z</dc:date>
    <item>
      <title>LPC546xx USB1 Examples</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-Examples/m-p/743662#M29987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm&amp;nbsp;developing a bare metal project on a custom board with a LPC54616 and need to get it working as a mass storage device using the USB1 controller.&lt;/P&gt;&lt;P&gt;Does anyone know if there are any LPC546xx&amp;nbsp;example projects which demonstrate using USB1, preferably as a device?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Matt...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2018 12:09:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-Examples/m-p/743662#M29987</guid>
      <dc:creator>mattskey</dc:creator>
      <dc:date>2018-03-28T12:09:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx USB1 Examples</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-Examples/m-p/743663#M29988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matt,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the SDK (which you can download from mcuxpresso.nxp.com) includes examples for both USB ports as devices. It doesn't really matter if you load the SDK for LPCXpresso54608 or&amp;nbsp;LPCXpresso54618 when it comes to USB. Look under boards\lpcxpresso54608\usb_examples, and you will see various mass storage class examples there. You need to set the header file to define USB1 or USB0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please mark this correct if it answers your question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Brendon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2018 15:47:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-Examples/m-p/743663#M29988</guid>
      <dc:creator>brendonslade</dc:creator>
      <dc:date>2018-03-29T15:47:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx USB1 Examples</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-Examples/m-p/743664#M29989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brendon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response. I have the boards\lpcxpresso54618\usb_examples\usb_device_msc_ramdisk_lite\bm example project but can't see any settings for USB0/1.&lt;SPAN style="font-size: small;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should I just need to change the values of &lt;/P&gt;&lt;P&gt;USB_DEVICE_CONFIG_LPCIP3511FS and &lt;/P&gt;&lt;P&gt;USB_DEVICE_CONFIG_LPCIP3511HS in usb_device_config.h?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or should I be looking at a different header file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry if this is a trivial question, I'm not familiar with MCUXpresso, Eclipse or USB so everything's a bit confusing at the moment. I have the OM13092 (LPCXpresso54608) board but am waiting for a connector before I can programme it. I then have&amp;nbsp;to get it working on custom hardware so any assistance is much appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Matt...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 11:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-Examples/m-p/743664#M29989</guid>
      <dc:creator>mattskey</dc:creator>
      <dc:date>2018-04-03T11:14:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx USB1 Examples</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-Examples/m-p/743665#M29990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the example:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;usb_examples_usb_rom_device_msc_ram_bm&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;there is a header file: app_usbd_cfg.h that contains the #define USE_USB0 or USE_USB1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The example that you're using may be similar.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 14:57:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-Examples/m-p/743665#M29990</guid>
      <dc:creator>patrickhudson</dc:creator>
      <dc:date>2018-04-03T14:57:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx USB1 Examples</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-Examples/m-p/743666#M29991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patrick,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the info. There doesn't seem to be an equivalent in the example I'm using but that should help working out what changes I need to make.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Matt...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 15:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB1-Examples/m-p/743666#M29991</guid>
      <dc:creator>mattskey</dc:creator>
      <dc:date>2018-04-03T15:20:32Z</dc:date>
    </item>
  </channel>
</rss>