<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Input clamp current in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Input-clamp-current/m-p/743470#M29978</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's the maximum input voltage level on an un-powered device?&lt;/P&gt;&lt;P&gt;What's the maximum input clamp current of an IO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I personally find the documentation on the input structure of LPC GPIO pins quite unclear.&lt;/P&gt;&lt;P&gt;Most pins are 5V tolerant, but only with Vdd present. But I can't seem to find the voltage levels when vdd is not present (LPC1317), see snapshot from the datasheet below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20209iE5DA417447A38EA5/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In another thread it is mentioned that the input structure is a normal input clamp but that can't be the case due to the 5V tolerant pins.&lt;/P&gt;&lt;P&gt;Also, the input clamp current is not specified both for analog and digital pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I follow the datasheet strictly this means that no signal can be connected to the micro-controller that isn't preceded by something that's on the same supply as the controller.&lt;/P&gt;&lt;P&gt;For example, the 3V3 rail of the controller could be short circuited or starting up while a 5V rail remains 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jan 2018 12:06:05 GMT</pubDate>
    <dc:creator>publius</dc:creator>
    <dc:date>2018-01-22T12:06:05Z</dc:date>
    <item>
      <title>Input clamp current</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Input-clamp-current/m-p/743470#M29978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's the maximum input voltage level on an un-powered device?&lt;/P&gt;&lt;P&gt;What's the maximum input clamp current of an IO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I personally find the documentation on the input structure of LPC GPIO pins quite unclear.&lt;/P&gt;&lt;P&gt;Most pins are 5V tolerant, but only with Vdd present. But I can't seem to find the voltage levels when vdd is not present (LPC1317), see snapshot from the datasheet below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20209iE5DA417447A38EA5/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In another thread it is mentioned that the input structure is a normal input clamp but that can't be the case due to the 5V tolerant pins.&lt;/P&gt;&lt;P&gt;Also, the input clamp current is not specified both for analog and digital pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I follow the datasheet strictly this means that no signal can be connected to the micro-controller that isn't preceded by something that's on the same supply as the controller.&lt;/P&gt;&lt;P&gt;For example, the 3V3 rail of the controller could be short circuited or starting up while a 5V rail remains 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jan 2018 12:06:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Input-clamp-current/m-p/743470#M29978</guid>
      <dc:creator>publius</dc:creator>
      <dc:date>2018-01-22T12:06:05Z</dc:date>
    </item>
    <item>
      <title>Re: Input clamp current</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Input-clamp-current/m-p/743471#M29979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi again,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, what are the specs for the open drain pins,&amp;nbsp; PIO0_4 &amp;amp; PIO0_5 for the LPC1317?&lt;/P&gt;&lt;P&gt;Are these 5V tolerant and I2C compliant? With or without supply?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could it be that the datasheet needs updating?&lt;/P&gt;&lt;P&gt;When I look in the datasheet of the LPC111x the open drain pins are mentioned but not for the LPC13xx:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25370iB5FD77B321546EA2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24907i6B6D01A5734869B5/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hopefully someone can help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some similar questions:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/428265"&gt;5V tolerant input&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/765563?commentID=765563#comment-765563" title="https://community.nxp.com/message/765563?commentID=765563#comment-765563"&gt;https://community.nxp.com/message/765563?commentID=765563#comment-765563&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/454563"&gt;I2C 5V Toterant&lt;/A&gt;&amp;nbsp;(with and without supply?)&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/750299?commentID=750299#comment-750299" title="https://community.nxp.com/message/750299?commentID=750299#comment-750299"&gt;https://community.nxp.com/message/750299?commentID=750299#comment-750299&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2018 09:12:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Input-clamp-current/m-p/743471#M29979</guid>
      <dc:creator>publius</dc:creator>
      <dc:date>2018-01-24T09:12:16Z</dc:date>
    </item>
    <item>
      <title>Re: Input clamp current</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Input-clamp-current/m-p/743472#M29980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;DIV style="white-space: pre-wrap; text-align: left; line-height: 1.75; font-size: 14px;"&gt;&lt;SPAN style="font-family: 'Microsoft YaHei', STXihei; background-color: #ffffff;"&gt;Thank you for your interest in NXP Semiconductor products and&amp;nbsp;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV style="white-space: pre-wrap; text-align: left; line-height: 1.75; font-size: 14px;"&gt;&lt;SPAN style="font-family: 'Microsoft YaHei', STXihei; background-color: #ffffff;"&gt;the opportunity to serve you.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV style="white-space: pre-wrap; text-align: left; line-height: 1.75; font-size: 14px;"&gt;&lt;SPAN style="font-family: 'Microsoft YaHei', STXihei; background-color: #ffffff;"&gt;Unfortunately, the datasheet doesn't contain the kind of information you want and I will report your inquiry for the Doc team.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV style="white-space: pre-wrap; text-align: left; line-height: 1.75; font-size: 14px;"&gt;&lt;SPAN style="font-family: 'Microsoft YaHei', STXihei; background-color: #ffffff;"&gt;Thanks for understanding.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV style="white-space: pre-wrap; text-align: left; line-height: 1.75; font-size: 14px;"&gt;Have a great day,&lt;/DIV&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jan 2018 08:02:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Input-clamp-current/m-p/743472#M29980</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-01-26T08:02:40Z</dc:date>
    </item>
    <item>
      <title>Re: Input clamp current</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Input-clamp-current/m-p/743473#M29981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response. Could you give an indication when to expect the data?&lt;/P&gt;&lt;P&gt;I'm currently designing a product with the LPC1317.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jan 2018 09:26:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Input-clamp-current/m-p/743473#M29981</guid>
      <dc:creator>publius</dc:creator>
      <dc:date>2018-01-26T09:26:31Z</dc:date>
    </item>
    <item>
      <title>Re: Input clamp current</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Input-clamp-current/m-p/743474#M29982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Sorry, I'm not clear with the exactly schedule of releasing the updated datasheet.&lt;/P&gt;&lt;P&gt;And I will inform if I get it.&lt;/P&gt;&lt;DIV style="white-space: pre-wrap; text-align: left; line-height: 1.75; font-size: 14px;"&gt;Have a great day,&lt;/DIV&gt;&lt;P&gt;TIC&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jan 2018 06:47:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Input-clamp-current/m-p/743474#M29982</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-01-29T06:47:57Z</dc:date>
    </item>
  </channel>
</rss>