<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックProcessor</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Processor/m-p/743407#M29976</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have your processor LPC1778FET208 CORTEX m3 16/32-Bit Microcontroller, 512KB Flash, 96KB RAM, 208-balls. Do you do the same BGA 208 Pins same pitch. We need more memory so we can hold about 10-20 Minutes of data in Flash. Much appreciated for your quick response.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Jun 2018 09:47:32 GMT</pubDate>
    <dc:creator>lesliehooker</dc:creator>
    <dc:date>2018-06-01T09:47:32Z</dc:date>
    <item>
      <title>Processor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Processor/m-p/743407#M29976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have your processor LPC1778FET208 CORTEX m3 16/32-Bit Microcontroller, 512KB Flash, 96KB RAM, 208-balls. Do you do the same BGA 208 Pins same pitch. We need more memory so we can hold about 10-20 Minutes of data in Flash. Much appreciated for your quick response.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jun 2018 09:47:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Processor/m-p/743407#M29976</guid>
      <dc:creator>lesliehooker</dc:creator>
      <dc:date>2018-06-01T09:47:32Z</dc:date>
    </item>
    <item>
      <title>Re: Processor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Processor/m-p/743408#M29977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Leslie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCU that is pin a pin compatible is the LPC4078 but the memory is also up to 512kB.&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/lpc-cortex-m-mcus/lpc4000-cortex-m4/32-bit-arm-cortex-m4-mcu-up-to-512-kb-flash-96-kb-sram-usb-device-host-otg-ethernet-emc-spifi:LPC4078FBD100?lang_cd=en" title="https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/lpc-cortex-m-mcus/lpc4000-cortex-m4/32-bit-arm-cortex-m4-mcu-up-to-512-kb-flash-96-kb-sram-usb-device-host-otg-ethernet-emc-spifi:LPC4078FBD100?lang_cd=en"&gt;LPC4078FBD100|ARM Cortex-M4|32-bit MCU|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you require more memory for the LPC1778 you can use a external memory, you can control it with the external memory controller peripheral (EMC).&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the &lt;STRONG&gt;LPC1773&lt;/STRONG&gt; you also have the SPI Flash interface (SPIFI).&amp;nbsp;The SPI Flash Interface allows low-cost serial flash memories to be connected to the Cortex-M3 processor with little performance penalty compared to parallel flash devices with higher pin count. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jun 2018 19:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Processor/m-p/743408#M29977</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-06-05T19:33:01Z</dc:date>
    </item>
  </channel>
</rss>