<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Internal weak-pull up resistance value</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-weak-pull-up-resistance-value/m-p/742593#M29939</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It's in the Datasheet Table 9 "Static Characteristics" Ipu Pull-up current. It is specified between 10µA and 85µA. It probably looks more like a constant current source, but as a resistor it somewhere between 39kΩ and 330kΩ.&lt;/P&gt;&lt;P&gt;Taking the worst case (85µA) and the maximum value for Vil (input low voltage of 0.3Vdd at 3.3V, which is 0.99V, then the largest resistor which will ensure pull-down is 0.99V/85µA = 11kΩ&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Apr 2018 20:14:30 GMT</pubDate>
    <dc:creator>ianbenton</dc:creator>
    <dc:date>2018-04-19T20:14:30Z</dc:date>
    <item>
      <title>Internal weak-pull up resistance value</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-weak-pull-up-resistance-value/m-p/742591#M29937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How much is the resistance value of internal weak-pull up in LPC802 GPIO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to keep a line which is connected to a MCU (LPC802) low level during it is in reset state. I believe that GPIO is configured as input function with internal weak-pull up resistance when the MCU is in reset state. Hear "reset state" means that the MCU's reset pin is low. Therefore, I consider placing an external pull-down resistance on the line and I'd like to know the resistance value of internal weak-pull up to calculate the appropriate external pull-down resistance value.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2018 17:27:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-weak-pull-up-resistance-value/m-p/742591#M29937</guid>
      <dc:creator>yoshiyukiokada</dc:creator>
      <dc:date>2018-03-27T17:27:37Z</dc:date>
    </item>
    <item>
      <title>Re: Internal weak-pull up resistance value</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-weak-pull-up-resistance-value/m-p/742592#M29938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yoshiyuki Okada,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Actually, the internal weak pull-up is the transistor, like the following picture:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20802i89FA3CB507DC6C88/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The simulated resistance value is about tens of K Ohm.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2018 02:55:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-weak-pull-up-resistance-value/m-p/742592#M29938</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-03-29T02:55:09Z</dc:date>
    </item>
    <item>
      <title>Re: Internal weak-pull up resistance value</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-weak-pull-up-resistance-value/m-p/742593#M29939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It's in the Datasheet Table 9 "Static Characteristics" Ipu Pull-up current. It is specified between 10µA and 85µA. It probably looks more like a constant current source, but as a resistor it somewhere between 39kΩ and 330kΩ.&lt;/P&gt;&lt;P&gt;Taking the worst case (85µA) and the maximum value for Vil (input low voltage of 0.3Vdd at 3.3V, which is 0.99V, then the largest resistor which will ensure pull-down is 0.99V/85µA = 11kΩ&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 20:14:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-weak-pull-up-resistance-value/m-p/742593#M29939</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2018-04-19T20:14:30Z</dc:date>
    </item>
  </channel>
</rss>