<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1778 PULL-UP</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-PULL-UP/m-p/739374#M29827</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yukinobu Hori,&lt;/P&gt;&lt;P&gt;&amp;nbsp;1. P5[2] and p5[3] is the open drain 5V tolerant pin, it needs an external pull up to provide output functionality, you can find it from the datasheet.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21079i9FD1BC3E493E3AA4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21210i57EED0B9DCD641E6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. P0[27], P0[28] is also the open drain pin.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21080iD8E355287126DA1C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21128iB0632A7DB3E1F488/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;3. But, P0[24], P0[25], P2[11],P2[12],P2[13] and P5[1] in default, it enables the PU,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21164iBEF5D91381FB931B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But it is the input function in default, you need to configure it to output by yourselves.These pin's Pull up is OK, please double check it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Mar 2018 05:35:15 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2018-03-29T05:35:15Z</dc:date>
    <item>
      <title>LPC1778 PULL-UP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-PULL-UP/m-p/739373#M29826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;P0 [24] to P0 [28] of LPC 1778,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;P2 [8] P2 [9] P2 [11] to P2 [13],&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;I want to set PULL-UP for P5 [1] to P5 [3].&lt;/SPAN&gt; &lt;SPAN&gt;.&lt;/SPAN&gt; &lt;SPAN&gt;.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;P0 [26], P2 [8], P2 [9], P5 [1] are OK.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Others are NG.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;If an external resistor (10 KΩ) is connected to P5 [2], P5 [3]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;It is confirmed that the operation is OK.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;If possible, GOOD is better without external resistance.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2018 01:32:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-PULL-UP/m-p/739373#M29826</guid>
      <dc:creator>yukinobuhori</dc:creator>
      <dc:date>2018-03-27T01:32:32Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 PULL-UP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-PULL-UP/m-p/739374#M29827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yukinobu Hori,&lt;/P&gt;&lt;P&gt;&amp;nbsp;1. P5[2] and p5[3] is the open drain 5V tolerant pin, it needs an external pull up to provide output functionality, you can find it from the datasheet.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21079i9FD1BC3E493E3AA4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21210i57EED0B9DCD641E6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. P0[27], P0[28] is also the open drain pin.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21080iD8E355287126DA1C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21128iB0632A7DB3E1F488/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;3. But, P0[24], P0[25], P2[11],P2[12],P2[13] and P5[1] in default, it enables the PU,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21164iBEF5D91381FB931B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But it is the input function in default, you need to configure it to output by yourselves.These pin's Pull up is OK, please double check it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2018 05:35:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-PULL-UP/m-p/739374#M29827</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-03-29T05:35:15Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 PULL-UP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-PULL-UP/m-p/739375#M29828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN&gt;Thank you very much.&lt;/SPAN&gt; &lt;SPAN&gt;I will proceed with it as reference.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;It was saved.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2018 05:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-PULL-UP/m-p/739375#M29828</guid>
      <dc:creator>yukinobuhori</dc:creator>
      <dc:date>2018-03-29T05:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 PULL-UP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-PULL-UP/m-p/739376#M29829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are welcome!&lt;/P&gt;&lt;P&gt;&amp;nbsp;If you still have question about this topic, please kindly let me know!&lt;/P&gt;&lt;P&gt;&amp;nbsp;If your question is solved, please help me to mark the correct answer, just to close this case, thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 01:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-PULL-UP/m-p/739376#M29829</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-04-03T01:27:07Z</dc:date>
    </item>
  </channel>
</rss>