<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPCXpresso LPC54618 mcu SPI</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-LPC54618-mcu-SPI/m-p/739302#M29822</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is with the functions you are selecting for each pin, you left everything with the Function 1 and this is wrong, since the functions change for each pin. You can refer the user manual of the LPC54618 (&lt;A href="https://www.nxp.com/docs/en/user-guide/UM10912.pdf" rel="nofollow noopener noreferrer noopener noreferrer" target="_blank"&gt;UM10912.pdf&lt;/A&gt;) in the chapter 10, table 256 you will find a table where you will see all the different functions for each pin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the SCK you are selecting port1_pin9 in function one. In the image below you can see that the correct function is the number 2 in order to be the SCK of the SPI1.&amp;nbsp;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;IMG alt="pastedImage_1.png" src="https://community.nxp.com/t5/image/serverpage/image-id/61508iF3D4B993498523A7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;For the MISO (&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;port2_pin4&lt;/SPAN&gt;), MOSI (&lt;SPAN&gt;port2_pin3&lt;/SPAN&gt;) and SSEL (&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;port2_pin5&lt;/SPAN&gt;) you selected function one. However, for these pins the correct function is number 3, as shown below.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;IMG alt="pastedImage_2.png" src="https://community.nxp.com/t5/image/serverpage/image-id/61509i28549C966E9FCBFF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Your code should look like the following.&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; uint32_t port1_pin9_config &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="comment token"&gt;/* Pin is configured as FC9_SCK */&lt;/SPAN&gt;
IOCON_PIO_FUNC2 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Selects pull-up function */&lt;/SPAN&gt;
IOCON_PIO_MODE_PULLUP &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Input function is not inverted */&lt;/SPAN&gt;
IOCON_PIO_INV_DI &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Enables digital function */&lt;/SPAN&gt;
IOCON_PIO_DIGITAL_EN &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Input filter disabled */&lt;/SPAN&gt;
IOCON_PIO_INPFILT_OFF &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Standard mode, output slew rate control is enabled */&lt;/SPAN&gt;
IOCON_PIO_SLEW_STANDARD &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Open drain is disabled */&lt;/SPAN&gt;
IOCON_PIO_OPENDRAIN_DI&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* PORT3 PIN20 (coords: N2) is configured as FC9_SCK */&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;IOCON_PinMuxSet&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;IOCON&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1U&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;9U&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; port1_pin9_config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

&lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; uint32_t port2_pin3_config &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="comment token"&gt;/* Pin is configured as FC9_RXD_SDA_MOSI */&lt;/SPAN&gt;
IOCON_PIO_FUNC3 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Selects pull-up function */&lt;/SPAN&gt;
IOCON_PIO_MODE_PULLUP &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Input function is not inverted */&lt;/SPAN&gt;
IOCON_PIO_INV_DI &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Enables digital function */&lt;/SPAN&gt;
IOCON_PIO_DIGITAL_EN &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Input filter disabled */&lt;/SPAN&gt;
IOCON_PIO_INPFILT_OFF &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Open drain is disabled */&lt;/SPAN&gt;
IOCON_PIO_OPENDRAIN_DI&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* PORT3 PIN21 (coords: P5) is configured as FC9_RXD_SDA_MOSI */&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;IOCON_PinMuxSet&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;IOCON&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;2U&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;3U&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; port2_pin3_config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;Also keep in mind that the example is using the Flexcomm9 since it's using SPI9. You want to use the SPI1, so, you will need to use the Flexcomm1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Nov 2020 14:04:10 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2020-11-02T14:04:10Z</dc:date>
    <item>
      <title>LPCXpresso LPC54618 mcu SPI</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-LPC54618-mcu-SPI/m-p/739301#M29821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have imported "Spi_interrupt_b2b_transfer_master" example from LPCxpresso sdk 2.3.1 example.&lt;/P&gt;&lt;P&gt;It was for SPI9 so I changed it to SPI1 as per my need. Even changed the pin in pinmux.c file as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;const uint32_t port1_pin9_config = (/* Pin is configured as FC9_SCK */&lt;BR /&gt; IOCON_PIO_FUNC1 |&lt;BR /&gt; /* Selects pull-up function */&lt;BR /&gt; IOCON_PIO_MODE_PULLUP |&lt;BR /&gt; /* Input function is not inverted */&lt;BR /&gt; IOCON_PIO_INV_DI |&lt;BR /&gt; /* Enables digital function */&lt;BR /&gt; IOCON_PIO_DIGITAL_EN |&lt;BR /&gt; /* Input filter disabled */&lt;BR /&gt; IOCON_PIO_INPFILT_OFF |&lt;BR /&gt; /* Standard mode, output slew rate control is enabled */&lt;BR /&gt; IOCON_PIO_SLEW_STANDARD |&lt;BR /&gt; /* Open drain is disabled */&lt;BR /&gt; IOCON_PIO_OPENDRAIN_DI);&lt;BR /&gt; /* PORT3 PIN20 (coords: N2) is configured as FC9_SCK */&lt;BR /&gt; IOCON_PinMuxSet(IOCON, 1U, 9U, port1_pin9_config);&lt;/P&gt;&lt;P&gt;const uint32_t port2_pin3_config = (/* Pin is configured as FC9_RXD_SDA_MOSI */&lt;BR /&gt; IOCON_PIO_FUNC1 |&lt;BR /&gt; /* Selects pull-up function */&lt;BR /&gt; IOCON_PIO_MODE_PULLUP |&lt;BR /&gt; /* Input function is not inverted */&lt;BR /&gt; IOCON_PIO_INV_DI |&lt;BR /&gt; /* Enables digital function */&lt;BR /&gt; IOCON_PIO_DIGITAL_EN |&lt;BR /&gt; /* Input filter disabled */&lt;BR /&gt; IOCON_PIO_INPFILT_OFF |&lt;BR /&gt; /* Open drain is disabled */&lt;BR /&gt; IOCON_PIO_OPENDRAIN_DI);&lt;BR /&gt; /* PORT3 PIN21 (coords: P5) is configured as FC9_RXD_SDA_MOSI */&lt;BR /&gt; IOCON_PinMuxSet(IOCON, 2U, 3U, port2_pin3_config);&lt;/P&gt;&lt;P&gt;const uint32_t port2_pin4_config = (/* Pin is configured as FC9_TXD_SCL_MISO */&lt;BR /&gt; IOCON_PIO_FUNC1 |&lt;BR /&gt; /* Selects pull-up function */&lt;BR /&gt; IOCON_PIO_MODE_PULLUP |&lt;BR /&gt; /* Input function is not inverted */&lt;BR /&gt; IOCON_PIO_INV_DI |&lt;BR /&gt; /* Enables digital function */&lt;BR /&gt; IOCON_PIO_DIGITAL_EN |&lt;BR /&gt; /* Input filter disabled */&lt;BR /&gt; IOCON_PIO_INPFILT_OFF |&lt;BR /&gt; /* Open drain is disabled */&lt;BR /&gt; IOCON_PIO_OPENDRAIN_DI);&lt;BR /&gt; /* PORT3 PIN22 (coords: N5) is configured as FC9_TXD_SCL_MISO */&lt;BR /&gt; IOCON_PinMuxSet(IOCON, 2U, 4U, port2_pin4_config);&lt;/P&gt;&lt;P&gt;const uint32_t port2_pin5_config = (/* Pin is configured as FC9_CTS_SDA_SSEL0 */&lt;BR /&gt; IOCON_PIO_FUNC1 |&lt;BR /&gt; /* Selects pull-up function */&lt;BR /&gt; IOCON_PIO_MODE_PULLUP |&lt;BR /&gt; /* Input function is not inverted */&lt;BR /&gt; IOCON_PIO_INV_DI |&lt;BR /&gt; /* Enables digital function */&lt;BR /&gt; IOCON_PIO_DIGITAL_EN |&lt;BR /&gt; /* Input filter disabled */&lt;BR /&gt; IOCON_PIO_INPFILT_OFF |&lt;BR /&gt; /* Standard mode, output slew rate control is enabled */&lt;BR /&gt; IOCON_PIO_SLEW_STANDARD |&lt;BR /&gt; /* Open drain is disabled */&lt;BR /&gt; IOCON_PIO_OPENDRAIN_DI);&lt;BR /&gt; /* PORT3 PIN30 (coords: K13) is configured as FC9_CTS_SDA_SSEL0 */&lt;BR /&gt; IOCON_PinMuxSet(IOCON, 2U, 5U, port2_pin5_config);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I am not getting any&amp;nbsp;clock in SPI CLK pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly guide.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2018 07:04:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-LPC54618-mcu-SPI/m-p/739301#M29821</guid>
      <dc:creator>shaheenshamshad</dc:creator>
      <dc:date>2018-05-31T07:04:35Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso LPC54618 mcu SPI</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-LPC54618-mcu-SPI/m-p/739302#M29822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is with the functions you are selecting for each pin, you left everything with the Function 1 and this is wrong, since the functions change for each pin. You can refer the user manual of the LPC54618 (&lt;A href="https://www.nxp.com/docs/en/user-guide/UM10912.pdf" rel="nofollow noopener noreferrer noopener noreferrer" target="_blank"&gt;UM10912.pdf&lt;/A&gt;) in the chapter 10, table 256 you will find a table where you will see all the different functions for each pin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the SCK you are selecting port1_pin9 in function one. In the image below you can see that the correct function is the number 2 in order to be the SCK of the SPI1.&amp;nbsp;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;IMG alt="pastedImage_1.png" src="https://community.nxp.com/t5/image/serverpage/image-id/61508iF3D4B993498523A7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;For the MISO (&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;port2_pin4&lt;/SPAN&gt;), MOSI (&lt;SPAN&gt;port2_pin3&lt;/SPAN&gt;) and SSEL (&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;port2_pin5&lt;/SPAN&gt;) you selected function one. However, for these pins the correct function is number 3, as shown below.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;IMG alt="pastedImage_2.png" src="https://community.nxp.com/t5/image/serverpage/image-id/61509i28549C966E9FCBFF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Your code should look like the following.&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; uint32_t port1_pin9_config &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="comment token"&gt;/* Pin is configured as FC9_SCK */&lt;/SPAN&gt;
IOCON_PIO_FUNC2 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Selects pull-up function */&lt;/SPAN&gt;
IOCON_PIO_MODE_PULLUP &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Input function is not inverted */&lt;/SPAN&gt;
IOCON_PIO_INV_DI &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Enables digital function */&lt;/SPAN&gt;
IOCON_PIO_DIGITAL_EN &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Input filter disabled */&lt;/SPAN&gt;
IOCON_PIO_INPFILT_OFF &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Standard mode, output slew rate control is enabled */&lt;/SPAN&gt;
IOCON_PIO_SLEW_STANDARD &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Open drain is disabled */&lt;/SPAN&gt;
IOCON_PIO_OPENDRAIN_DI&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* PORT3 PIN20 (coords: N2) is configured as FC9_SCK */&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;IOCON_PinMuxSet&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;IOCON&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1U&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;9U&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; port1_pin9_config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

&lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; uint32_t port2_pin3_config &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="comment token"&gt;/* Pin is configured as FC9_RXD_SDA_MOSI */&lt;/SPAN&gt;
IOCON_PIO_FUNC3 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Selects pull-up function */&lt;/SPAN&gt;
IOCON_PIO_MODE_PULLUP &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Input function is not inverted */&lt;/SPAN&gt;
IOCON_PIO_INV_DI &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Enables digital function */&lt;/SPAN&gt;
IOCON_PIO_DIGITAL_EN &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Input filter disabled */&lt;/SPAN&gt;
IOCON_PIO_INPFILT_OFF &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Open drain is disabled */&lt;/SPAN&gt;
IOCON_PIO_OPENDRAIN_DI&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* PORT3 PIN21 (coords: P5) is configured as FC9_RXD_SDA_MOSI */&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;IOCON_PinMuxSet&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;IOCON&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;2U&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;3U&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; port2_pin3_config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;Also keep in mind that the example is using the Flexcomm9 since it's using SPI9. You want to use the SPI1, so, you will need to use the Flexcomm1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:04:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-LPC54618-mcu-SPI/m-p/739302#M29822</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2020-11-02T14:04:10Z</dc:date>
    </item>
  </channel>
</rss>