<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC54608 - Can USB0 support HS as a Device ? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736331#M29750</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kevin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry, I'm just using the ROM API to get a single HS USB device using the internal transceiver on the LPC5461x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best wishes,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Feb 2018 09:27:05 GMT</pubDate>
    <dc:creator>andyjackson</dc:creator>
    <dc:date>2018-02-14T09:27:05Z</dc:date>
    <item>
      <title>LPC54608 - Can USB0 support HS as a Device ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736320#M29739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;H1 style="color: #646464; background-color: #ffffff; border: 0px; font-weight: 200; font-size: 2rem;"&gt;LPC54608 USB0 HS Device Mode question&lt;/H1&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a 54608 design, I need USB0 to operate as a HS device and USB1 to operate as HS Host.&lt;/P&gt;&lt;P&gt;Can the USB0 operate in HS mode (device only) ?. I don't need OTG for any of it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is USB0 limited to FS because its only a FS PHY ? Or can it operate as a HS Device as well ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently i have USB1 in HS as a host running with, USB0 in FS operating as a device (ROM API mode).&lt;/P&gt;&lt;P&gt;I think the ROM API limits this to FS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the ROM API allows HS for USB0 - that would be great, but i don't think it will.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I couldn't find any example code where USB0 is used as a HS Device (or Host) ? Only USB1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I have to move to a ULPI interface to get USB0 to operate in HS ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jan 2018 20:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736320#M29739</guid>
      <dc:creator>k2</dc:creator>
      <dc:date>2018-01-19T20:58:55Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 - Can USB0 support HS as a Device ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736321#M29740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kevin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; USB0 in LPC54608 is just the full-speed device or host controller, it can't support the High-speed device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; USB1 can used for High-speed mode, USB0 module don't have the high speed function, it is not the ROM API problem, USB0 hardware can't support it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jan 2018 03:14:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736321#M29740</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-01-23T03:14:29Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 - Can USB0 support HS as a Device ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736322#M29741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you clarify the situation with USB1 - can it be used in HS mode with the ROM API and if so, where can I find some example code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jan 2018 16:59:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736322#M29741</guid>
      <dc:creator>andyjackson</dc:creator>
      <dc:date>2018-01-23T16:59:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 - Can USB0 support HS as a Device ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736323#M29742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you know of any development boards that have 2 HS PHY's ?&lt;/P&gt;&lt;P&gt;I see chips that 2 HS controllers - like the 43XX series - but none have 2 HS PHYS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess what im looking for is a 2nd HS PHY via a ULPI chip.&lt;/P&gt;&lt;P&gt;I can't find anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ideally what I need is using USB1 (Host mode ) in HS, and a second HS Device (probably need a ULPI chip to add the HS PHY).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you know of any boards that have this ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alternatively - do you if there is a way the FS Device (using ROM API) can support 512 size packets ?&lt;/P&gt;&lt;P&gt;That would move me along until i can design in a ULPI interface on my board.&lt;/P&gt;&lt;P&gt;Is there a ULPI app note or code example anywhere ? To show how this interfaces with a device stack ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kevin&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jan 2018 17:47:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736323#M29742</guid>
      <dc:creator>k2</dc:creator>
      <dc:date>2018-01-29T17:47:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 - Can USB0 support HS as a Device ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736324#M29743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kerry,&lt;/P&gt;&lt;P&gt;I dont see the LPC 546XX&amp;nbsp; family supporting ULPI ?&lt;/P&gt;&lt;P&gt;Can you confirm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because the 546XX doesnt support ULPI, my design will now move to the LPC1833 (BD 208) to support a ULPI interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the LPC1833 family - Does the ROM API support the ULPI seemlessly ?&lt;/P&gt;&lt;P&gt;Or is there special code that needs to be implemented to make the USB1 port work as HS.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Its unclear to me how adding a ULPI chip such as the microchip will be plug and play ?&lt;/P&gt;&lt;P&gt;IS there any example code or APP note outlining how to implement the ULPI ?&lt;/P&gt;&lt;P&gt;I assume i'll be enabling the ULPI interface in the GPIO setting/functions, after that how is the ULPI seen ?&lt;/P&gt;&lt;P&gt;Does the USB1 port map into a different address for the ULPI to be seen ?&lt;/P&gt;&lt;P&gt;I assume there are some commands that need to be sent to this ULPI chip ?&lt;/P&gt;&lt;P&gt;Is that all done for me ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Feb 2018 18:22:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736324#M29743</guid>
      <dc:creator>k2</dc:creator>
      <dc:date>2018-02-05T18:22:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 - Can USB0 support HS as a Device ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736325#M29744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Kerry,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;I dont see the LPC 546XX&amp;nbsp; family supporting ULPI ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Can you confirm.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Because the 546XX doesnt support ULPI, my design will now move to the LPC1833 (BD 208) to support a ULPI interface.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;For the LPC1833 family - Does the ROM API support the ULPI seemlessly ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Or is there special code that needs to be implemented to make the USB1 port work as HS.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Its unclear to me how adding a ULPI chip such as the microchip will be plug and play ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;IS there any example code or APP note outlining how to implement the ULPI ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;I assume i'll be enabling the ULPI interface in the GPIO setting/functions, after that how is the ULPI seen ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Does the USB1 port map into a different address for the ULPI to be seen ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;I assume there are some commands that need to be sent to this ULPI chip ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Is that all done for me ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Feb 2018 18:23:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736325#M29744</guid>
      <dc:creator>k2</dc:creator>
      <dc:date>2018-02-05T18:23:07Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 - Can USB0 support HS as a Device ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736326#M29745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andy Jackson,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Sorry for my later reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; From the ROM API function description, I think it support the USB1, but now I don't have the according API code for your reference.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please don't worry, we also have some other USB1 sample code for your reference.&lt;/P&gt;&lt;P&gt;1. ppt&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-334179"&gt;17_LPC546xx USB.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-334206"&gt;HOT_17_USB.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. according sample code&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/448799"&gt;LPC546xx Hands-on projects&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to the training ppt and code.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Feb 2018 03:31:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736326#M29745</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-02-07T03:31:55Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 - Can USB0 support HS as a Device ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736327#M29746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kevin,&lt;/P&gt;&lt;P&gt;1. LPC54608 ULPI&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please refer to this LPC546XX USB training document:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-334179"&gt;17_LPC546xx USB.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can find this information:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/515i4DB80A2F5DCA30FA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2. LPC1833 ULPI&lt;/P&gt;&lt;P&gt;&amp;nbsp; The LPC1833 ULPI interface support info is in the following table:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/552i44641C890E9B7F03/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now answer your several questions about the LPC1833 ULPI:&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;1)For the LPC1833 family - Does the ROM API support the ULPI seemlessly ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Or is there special code that needs to be implemented to make the USB1 port work as HS.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Answer: About the LPC1833 ULPI API support question, I didn't find any information about the ULPI in the usb ROM API, so I think you need to use the USB driver control it.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;You can check the LPC1833 user manual about the ULPI usage:&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;SPAN&gt; &lt;A data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fdocuments%2Fuser_manual%2FUM10430.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/documents/user_manual/UM10430.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/635i9ACD9658EC593989/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_8.png" alt="pastedImage_8.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;SPAN&gt;Please take care, in LPC18xx series, USB0 support the high speed PHY, you don't need to connect external PHY, but USB1 in high speed, it need to use the ULPI connect with the external high speed PHY.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;2)Its unclear to me how adding a ULPI chip such as the microchip will be plug and play ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Answer: check item 1) and the user manual.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;3)IS there any example code or APP note outlining how to implement the ULPI ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Answer:Please check this application note:AN11309&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN11309.zip?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="https://www.nxp.com/docs/en/application-note/AN11309.zip?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;https://www.nxp.com/docs/en/application-note/AN11309.zip&lt;/A&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;It has the document and the sample code.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;4)I assume i'll be enabling the ULPI interface in the GPIO setting/functions, after that how is the ULPI seen ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;5)Does the USB1 port map into a different address for the ULPI to be seen ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;6)I assume there are some commands that need to be sent to this ULPI chip ?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Answer: All 4) 5) 6), please refer to the AN11309 and the chip user manual.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Wish it helps you!&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Feb 2018 06:17:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736327#M29746</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-02-07T06:17:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 - Can USB0 support HS as a Device ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736328#M29747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Couldn't open the LPC546XX USB.pdf link - says unauthorized ...&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I couldnt find anything that says the&amp;nbsp; LPC546XX family will support ULPI&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;like the LPC43XX and LPC1837/57 do.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;If it does that would be great.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I'm now switching over to and laying out a LPC1857 ULPI design with the USB3343 chip for the PHY.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I found the AN11309 appnote last week. Thanks anyways.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Has anyone tried this with the JBD208 package (Leaded).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;The app note example uses the 256 pin BGA package using PC0-PC8 pins.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I assume i can set the ULPI clocks to P8 and PB ports in the same way as in the BGA package.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;My preference would be to stay with the 546XX family because i have a working design already,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt; but i couldn't find it saying it supported the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;ULPI interface anywhere in the datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt; I couldn't open your links.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Is the short answer - that the LPC546XX family will not support ULPI ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;In the short term i'm redesigning the ULPI interface with the 1857/4357 chip.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hoping the leaded 208 pin package will work the same as the BGA 256 pin package.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Easier to build the 208 Pin version than the BGA version. Although i can place BGA's&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;if i need to.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Any reason you can think of to not use the 208 pin version for a ULPI design ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Im using P8-3 thru P8-8 and PB-1 thru PB-6 for the ULPI pins. It all seemed to map ok in the datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Would have been cool if they could have squeezed this in a smaller footprint.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;This 208 package is really huge.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Tell NXP to create a version that has dual HS ports. Strip out the Ethernet, LCD, ADC, functions to fit it in.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;My designs are USB centric. I mainly use HS USB, I2C and I2S functionality.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Feb 2018 19:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736328#M29747</guid>
      <dc:creator>k2</dc:creator>
      <dc:date>2018-02-07T19:41:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 - Can USB0 support HS as a Device ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736329#M29748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The example was exactly what I needed and I now have USB1 working via the ROM API - thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best wishes,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Feb 2018 13:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736329#M29748</guid>
      <dc:creator>andyjackson</dc:creator>
      <dc:date>2018-02-13T13:49:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 - Can USB0 support HS as a Device ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736330#M29749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Andy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you running USB1 in HS with a ULPI interface ?&lt;/P&gt;&lt;P&gt;I'm designing in an ULPI interface to get 2 HS ports (Host + Device) with the USB3343 chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kevin&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Feb 2018 01:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736330#M29749</guid>
      <dc:creator>k2</dc:creator>
      <dc:date>2018-02-14T01:17:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 - Can USB0 support HS as a Device ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736331#M29750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kevin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry, I'm just using the ROM API to get a single HS USB device using the internal transceiver on the LPC5461x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best wishes,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Feb 2018 09:27:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-Can-USB0-support-HS-as-a-Device/m-p/736331#M29750</guid>
      <dc:creator>andyjackson</dc:creator>
      <dc:date>2018-02-14T09:27:05Z</dc:date>
    </item>
  </channel>
</rss>