<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックHas anybody found a solution for using multiple LPCLink-2 adaptors connected through a USB hub, It seems that with the default settings prevent a second LPC-Link2 from enumerating</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Has-anybody-found-a-solution-for-using-multiple-LPCLink-2/m-p/731209#M29561</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It would appear that when programming the LPC-Link2 with the Segger code all devices are given the same serial number , 61000000, so the debugger is unable to distinguish them properly.&lt;/P&gt;&lt;P&gt;When using the CMSIS-DAP code it is not possible to connect 2 debuggers through a USB Hub since the second debugger reports insufficient system resources when using a single hub, but works when connected to a different root hub on the PC.&lt;/P&gt;&lt;P&gt;Also when programming multiple debuggers with the CMSIS-DAP code the script reports the same "Unique identifier" for all devices and it's not correct for any of them.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jan 2018 09:12:43 GMT</pubDate>
    <dc:creator>philyoung</dc:creator>
    <dc:date>2018-01-17T09:12:43Z</dc:date>
    <item>
      <title>Has anybody found a solution for using multiple LPCLink-2 adaptors connected through a USB hub, It seems that with the default settings prevent a second LPC-Link2 from enumerating</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Has-anybody-found-a-solution-for-using-multiple-LPCLink-2/m-p/731209#M29561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It would appear that when programming the LPC-Link2 with the Segger code all devices are given the same serial number , 61000000, so the debugger is unable to distinguish them properly.&lt;/P&gt;&lt;P&gt;When using the CMSIS-DAP code it is not possible to connect 2 debuggers through a USB Hub since the second debugger reports insufficient system resources when using a single hub, but works when connected to a different root hub on the PC.&lt;/P&gt;&lt;P&gt;Also when programming multiple debuggers with the CMSIS-DAP code the script reports the same "Unique identifier" for all devices and it's not correct for any of them.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 09:12:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Has-anybody-found-a-solution-for-using-multiple-LPCLink-2/m-p/731209#M29561</guid>
      <dc:creator>philyoung</dc:creator>
      <dc:date>2018-01-17T09:12:43Z</dc:date>
    </item>
    <item>
      <title>Re: Has anybody found a solution for using multiple LPCLink-2 adaptors connected through a USB hub, It seems that with the default settings prevent a second LPC-Link2 from enumerating</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Has-anybody-found-a-solution-for-using-multiple-LPCLink-2/m-p/731210#M29562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try using the non-bridged version of the current LPC-Link2 CMSIS-DAP firmware:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389141"&gt;Using Multiple LPC-Link2 debug probes&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/630661"&gt;https://community.nxp.com/message/630661&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 11:48:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Has-anybody-found-a-solution-for-using-multiple-LPCLink-2/m-p/731210#M29562</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-01-17T11:48:16Z</dc:date>
    </item>
    <item>
      <title>Re: Has anybody found a solution for using multiple LPCLink-2 adaptors connected through a USB hub, It seems that with the default settings prevent a second LPC-Link2 from enumerating</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Has-anybody-found-a-solution-for-using-multiple-LPCLink-2/m-p/731211#M29563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, this seems to work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 14:00:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Has-anybody-found-a-solution-for-using-multiple-LPCLink-2/m-p/731211#M29563</guid>
      <dc:creator>philyoung</dc:creator>
      <dc:date>2018-01-17T14:00:18Z</dc:date>
    </item>
  </channel>
</rss>