<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 DUAL USB example code ?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/DUAL-USB-example-code/m-p/730638#M29549</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking for some USB dual port example code. (I'm using the LPC4337)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want USB0 to be HOST from EHCI driver (Flash based) .&lt;/P&gt;&lt;P&gt;I'm using USB1 as a HS device in ROM API (using ULPI), so&amp;nbsp; i have this part done.&lt;/P&gt;&lt;P&gt;Looking to now add the USB0 HS EHCI Host.&lt;/P&gt;&lt;P&gt;Isn't there a CMIS driver somewhere for USB0 Host ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wasn't there a DUAL HS Explorer board using ULPI being sold awhile back ?&lt;/P&gt;&lt;P&gt;Seems there should be some Demo code for that ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anybody done this ? I think someone has.&lt;/P&gt;&lt;P&gt;I assume the ROM API can't support both a HS HOST and HS DEVICE simultaneously ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please point me to a USB0 Host driver example that isn't using the ROM API.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've used the EHCI driver in the LPC54608. Would that back port to the LPC4337 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kevin&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Mar 2018 08:00:06 GMT</pubDate>
    <dc:creator>k2</dc:creator>
    <dc:date>2018-03-23T08:00:06Z</dc:date>
    <item>
      <title>DUAL USB example code ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DUAL-USB-example-code/m-p/730638#M29549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking for some USB dual port example code. (I'm using the LPC4337)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want USB0 to be HOST from EHCI driver (Flash based) .&lt;/P&gt;&lt;P&gt;I'm using USB1 as a HS device in ROM API (using ULPI), so&amp;nbsp; i have this part done.&lt;/P&gt;&lt;P&gt;Looking to now add the USB0 HS EHCI Host.&lt;/P&gt;&lt;P&gt;Isn't there a CMIS driver somewhere for USB0 Host ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wasn't there a DUAL HS Explorer board using ULPI being sold awhile back ?&lt;/P&gt;&lt;P&gt;Seems there should be some Demo code for that ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anybody done this ? I think someone has.&lt;/P&gt;&lt;P&gt;I assume the ROM API can't support both a HS HOST and HS DEVICE simultaneously ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please point me to a USB0 Host driver example that isn't using the ROM API.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've used the EHCI driver in the LPC54608. Would that back port to the LPC4337 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kevin&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Mar 2018 08:00:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DUAL-USB-example-code/m-p/730638#M29549</guid>
      <dc:creator>k2</dc:creator>
      <dc:date>2018-03-23T08:00:06Z</dc:date>
    </item>
    <item>
      <title>Re: DUAL USB example code ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DUAL-USB-example-code/m-p/730639#M29550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check below thread about LPC43xx USB0 EHCI driver example:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/472522"&gt;https://community.nxp.com/thread/472522 &lt;/A&gt;&lt;/P&gt;&lt;P&gt;There is an application note AN11309 about using USB1 as high speed USB host with ULPI interface.&lt;/P&gt;&lt;P&gt;Please download LPC4357 USB Certification Support Pack(REV 1.0) from &lt;A href="https://www.nxp.com/downloads/en/lab-test-software/LPC4357-USB-Certification-Support-Pack.zip"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2018 09:04:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DUAL-USB-example-code/m-p/730639#M29550</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-03-29T09:04:36Z</dc:date>
    </item>
  </channel>
</rss>