<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC802: Can overwrite the BootROM by using self special bootloader functionality?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-Can-overwrite-the-BootROM-by-using-self-special/m-p/727883#M29435</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As the name "ROM" says, this memory area is Read-only. You can't erase and reprogram it.&lt;/P&gt;&lt;P&gt;The Boot ROM is an essential part of the chip startup procedure, therefore it is protected after programming in production.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 May 2018 07:56:14 GMT</pubDate>
    <dc:creator>bernhardfink</dc:creator>
    <dc:date>2018-05-07T07:56:14Z</dc:date>
    <item>
      <title>LPC802: Can overwrite the BootROM by using self special bootloader functionality?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-Can-overwrite-the-BootROM-by-using-self-special/m-p/727882#M29434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am fresh to LPC802 and i have been go through the datasheet for NXP LPC802.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I notice that there is a section for Boot ROM which locate at 0x0F00 0000 to 0x0F00 1FFF as show as below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12571i2207FA027E5D9A44/image-size/large?v=v2&amp;amp;px=999" title="memoryMap.jpg" alt="memoryMap.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let say i got one special bootloader's function which going to use special protocol to run the function, capture the data over UART and flash to internal flash memory, but i notice that this will not match with the current ISP/IAP functionality.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My idea is to clear this Boot ROM section and overwrite with my unique bootloader, is this be possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just worry this section is unable for user to clear on it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please advise.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;kj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 May 2018 15:23:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-Can-overwrite-the-BootROM-by-using-self-special/m-p/727882#M29434</guid>
      <dc:creator>kjteo</dc:creator>
      <dc:date>2018-05-05T15:23:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC802: Can overwrite the BootROM by using self special bootloader functionality?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-Can-overwrite-the-BootROM-by-using-self-special/m-p/727883#M29435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As the name "ROM" says, this memory area is Read-only. You can't erase and reprogram it.&lt;/P&gt;&lt;P&gt;The Boot ROM is an essential part of the chip startup procedure, therefore it is protected after programming in production.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 May 2018 07:56:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-Can-overwrite-the-BootROM-by-using-self-special/m-p/727883#M29435</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2018-05-07T07:56:14Z</dc:date>
    </item>
  </channel>
</rss>