<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Unexpected DMA Behaviour with LPC1778 Two</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unexpected-DMA-Behaviour-with-LPC1778-Two/m-p/518800#M2864</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Mon Jan 14 22:18:35 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using LPCXpresso 4.3 to debug (because I am not convinced of v5 stability yet) on WinXP Prof SP3 (32 bit)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC1778 Custom PCB&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I forgot to set the EnableDMA bit in the FIFO register when I set up my uart (Uart0)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Then I setup the RX DMA channel as if I had.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The surprising thing is that the RX DMA is working as expected -- i.e. received characters can be seen in the DMA&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;buffer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone explain this or othwerwise shed light on the issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;See also my thread "Unexpected DMA Behaviour with LPC1778".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:35:36 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:35:36Z</dc:date>
    <item>
      <title>Unexpected DMA Behaviour with LPC1778 Two</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unexpected-DMA-Behaviour-with-LPC1778-Two/m-p/518800#M2864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Mon Jan 14 22:18:35 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using LPCXpresso 4.3 to debug (because I am not convinced of v5 stability yet) on WinXP Prof SP3 (32 bit)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC1778 Custom PCB&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I forgot to set the EnableDMA bit in the FIFO register when I set up my uart (Uart0)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Then I setup the RX DMA channel as if I had.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The surprising thing is that the RX DMA is working as expected -- i.e. received characters can be seen in the DMA&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;buffer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone explain this or othwerwise shed light on the issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;See also my thread "Unexpected DMA Behaviour with LPC1778".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unexpected-DMA-Behaviour-with-LPC1778-Two/m-p/518800#M2864</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:35:36Z</dc:date>
    </item>
  </channel>
</rss>