<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC4330 recognize High Speed Device as Low Speed Device in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-recognize-High-Speed-Device-as-Low-Speed-Device/m-p/709623#M28639</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thanks for your advice.&amp;nbsp; Finally I found another solution. What I did was,&lt;/P&gt;&lt;P&gt;&amp;nbsp;at the interrupt routine of "detect device connection", I forced to the port "High Speed" by PORT_SC1H "force High Speed test mode" then return to "Normal mode" by resetting&amp;nbsp; the bit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;This workaround was not perfect.&amp;nbsp; Sometime the device was configured to "Low Speed", so I added retry.&lt;/P&gt;&lt;P&gt;&amp;nbsp;I found it worked well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The device needs 500mA, I guess it needs time to be stable from power on, but the USB controller would try to get the status of the device before the device become stable.&amp;nbsp; If so this problem could happen in other big current eater devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I know more general and smarter way is to use USB hub, but this time I need to adapt only the device, so I din't use hub solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yasushi Aoyama&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Oct 2017 06:44:44 GMT</pubDate>
    <dc:creator>yasushiaoyama</dc:creator>
    <dc:date>2017-10-20T06:44:44Z</dc:date>
    <item>
      <title>LPC4330 recognize High Speed Device as Low Speed Device</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-recognize-High-Speed-Device-as-Low-Speed-Device/m-p/709621#M28637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I'm developing USB host function for USB high speed devices. &amp;nbsp;I have a trouble of recognizing USB speed. &amp;nbsp;LPC4330 recognize some high speed device as low speed devices. &amp;nbsp;I'd appreciate if somebody could advice me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Environment) H/W: LPC4330 Explore Board&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;SW: &amp;nbsp;lpcopen_3_01_lpcxpresso_ngx_xplorer_4330&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Problem) Some high speed device is recognized low speed device. Some device can be recognized as high speed device correctly. &amp;nbsp;It's depends on device model. &amp;nbsp;Not depends on timing nor individual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I checked PORTSC1_H register when port status change occurs.(Device Connect)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;(A)The high speed device correctly recognized, PORTSC1_H value is 0x30001803.&lt;/P&gt;&lt;P&gt;&amp;nbsp; PSPD(b27:26) = 00 &amp;nbsp;Full Speed&lt;/P&gt;&lt;P&gt;&amp;nbsp; LS(b11:10)= 10: Not Low Speed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;(B)The high speed device recognized as Low speed,&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;PORTSC1_H value is 0x34001803&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; PSPD(b27:26) = 01 &amp;nbsp;Low Speed&lt;/P&gt;&lt;P&gt;&amp;nbsp; LS(b11:10)= 10: Not Low Speed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In (A) case, after bus reset, device chirp and hub chirp occurs and the device becomes High speed device.&lt;/P&gt;&lt;P&gt;In (B) case, after bus reset, device chirp occurs but hub chirp doesn't occur, the device remain low speed device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yasushi Aoyama&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 04:14:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-recognize-High-Speed-Device-as-Low-Speed-Device/m-p/709621#M28637</guid>
      <dc:creator>yasushiaoyama</dc:creator>
      <dc:date>2017-09-21T04:14:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4330 recognize High Speed Device as Low Speed Device</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-recognize-High-Speed-Device-as-Low-Speed-Device/m-p/709622#M28638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yasushi Aoyama,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which LPCOpen example are you using? I see you mention that you are using a HUB, is it the same problem if you remove the hub and connect the USB device directly to the host?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried using a USB analyzer to log the information and see if the Device is the one failing or is it is the Host?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Oct 2017 20:07:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-recognize-High-Speed-Device-as-Low-Speed-Device/m-p/709622#M28638</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-10-02T20:07:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4330 recognize High Speed Device as Low Speed Device</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-recognize-High-Speed-Device-as-Low-Speed-Device/m-p/709623#M28639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thanks for your advice.&amp;nbsp; Finally I found another solution. What I did was,&lt;/P&gt;&lt;P&gt;&amp;nbsp;at the interrupt routine of "detect device connection", I forced to the port "High Speed" by PORT_SC1H "force High Speed test mode" then return to "Normal mode" by resetting&amp;nbsp; the bit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;This workaround was not perfect.&amp;nbsp; Sometime the device was configured to "Low Speed", so I added retry.&lt;/P&gt;&lt;P&gt;&amp;nbsp;I found it worked well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The device needs 500mA, I guess it needs time to be stable from power on, but the USB controller would try to get the status of the device before the device become stable.&amp;nbsp; If so this problem could happen in other big current eater devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I know more general and smarter way is to use USB hub, but this time I need to adapt only the device, so I din't use hub solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yasushi Aoyama&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Oct 2017 06:44:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-recognize-High-Speed-Device-as-Low-Speed-Device/m-p/709623#M28639</guid>
      <dc:creator>yasushiaoyama</dc:creator>
      <dc:date>2017-10-20T06:44:44Z</dc:date>
    </item>
  </channel>
</rss>