<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC4337 running at 200MHz, 45 degrees C. Is this normal temperature?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-running-at-200MHz-45-degrees-C-Is-this-normal/m-p/709219#M28606</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Running LPC4337 at 200 MHz, and the case is very warm, measuring 45 degrees C or more. &amp;nbsp;When the clock is reduced to 100 MHz, it runs much cooler. &amp;nbsp;Is this a normal temperature range for 200 MHz?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Sep 2017 19:13:37 GMT</pubDate>
    <dc:creator>danschultz</dc:creator>
    <dc:date>2017-09-20T19:13:37Z</dc:date>
    <item>
      <title>LPC4337 running at 200MHz, 45 degrees C. Is this normal temperature?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-running-at-200MHz-45-degrees-C-Is-this-normal/m-p/709219#M28606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Running LPC4337 at 200 MHz, and the case is very warm, measuring 45 degrees C or more. &amp;nbsp;When the clock is reduced to 100 MHz, it runs much cooler. &amp;nbsp;Is this a normal temperature range for 200 MHz?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2017 19:13:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-running-at-200MHz-45-degrees-C-Is-this-normal/m-p/709219#M28606</guid>
      <dc:creator>danschultz</dc:creator>
      <dc:date>2017-09-20T19:13:37Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4337 running at 200MHz, 45 degrees C. Is this normal temperature?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-running-at-200MHz-45-degrees-C-Is-this-normal/m-p/709220#M28607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Absolutely! This chip is done in a 90nm technology, at 200MHz the chip will get warm.&lt;/P&gt;&lt;P&gt;Depending on the number of peripherals you run, it also might get hot.&lt;/P&gt;&lt;P&gt;What you should check: &amp;nbsp;the clock tree for all peripherals is enabled by default after reset. So you should switch off everything in the beginning (except the core of course :-) and then switch the clocks for the needed peripheral blocks on step by step in your system initialization.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 09:11:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-running-at-200MHz-45-degrees-C-Is-this-normal/m-p/709220#M28607</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2017-09-21T09:11:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4337 running at 200MHz, 45 degrees C. Is this normal temperature?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-running-at-200MHz-45-degrees-C-Is-this-normal/m-p/709221#M28608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response. &amp;nbsp; I am indeed using several peripherals, including all of the timer peripherals, all with a divide by one.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 14:19:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-running-at-200MHz-45-degrees-C-Is-this-normal/m-p/709221#M28608</guid>
      <dc:creator>danschultz</dc:creator>
      <dc:date>2017-09-21T14:19:53Z</dc:date>
    </item>
  </channel>
</rss>