<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC824 - IRC - quoted 12MHz +/- 1.5% in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-IRC-quoted-12MHz-1-5/m-p/706096#M28469</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any avalible graphed data showing typical curves?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vs Voltage&lt;/P&gt;&lt;P&gt;Vs Temp&lt;/P&gt;&lt;P&gt;Vs ageing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also is the following qualified? i.e. what is the accuracy below 2.7V?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"Conditions: Frequency values are typical values. 12 MHz  1.5 % accuracy is guaranteed for&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;2.7 V  VDD  3.6 V. Variations between parts may cause the IRC to fall outside the 12 MHz &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1.5 % accuracy specification for voltages below 2.7 V."&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Oct 2017 15:16:16 GMT</pubDate>
    <dc:creator>sanders7284</dc:creator>
    <dc:date>2017-10-13T15:16:16Z</dc:date>
    <item>
      <title>LPC824 - IRC - quoted 12MHz +/- 1.5%</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-IRC-quoted-12MHz-1-5/m-p/706096#M28469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any avalible graphed data showing typical curves?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vs Voltage&lt;/P&gt;&lt;P&gt;Vs Temp&lt;/P&gt;&lt;P&gt;Vs ageing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also is the following qualified? i.e. what is the accuracy below 2.7V?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"Conditions: Frequency values are typical values. 12 MHz  1.5 % accuracy is guaranteed for&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;2.7 V  VDD  3.6 V. Variations between parts may cause the IRC to fall outside the 12 MHz &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1.5 % accuracy specification for voltages below 2.7 V."&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Oct 2017 15:16:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-IRC-quoted-12MHz-1-5/m-p/706096#M28469</guid>
      <dc:creator>sanders7284</dc:creator>
      <dc:date>2017-10-13T15:16:16Z</dc:date>
    </item>
  </channel>
</rss>