<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Un-bonded Pins in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Un-bonded-Pins/m-p/704227#M28356</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPC 8xx devices...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know if it is possible to use unbonded pins for routing via the SWM block and various block inputs WITHOUT using existing bonded pins? Are these unbonded I/Os still available on packages with low pin count?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Sep 2017 18:36:05 GMT</pubDate>
    <dc:creator>bob_walker</dc:creator>
    <dc:date>2017-09-14T18:36:05Z</dc:date>
    <item>
      <title>Un-bonded Pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Un-bonded-Pins/m-p/704227#M28356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPC 8xx devices...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know if it is possible to use unbonded pins for routing via the SWM block and various block inputs WITHOUT using existing bonded pins? Are these unbonded I/Os still available on packages with low pin count?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Sep 2017 18:36:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Un-bonded-Pins/m-p/704227#M28356</guid>
      <dc:creator>bob_walker</dc:creator>
      <dc:date>2017-09-14T18:36:05Z</dc:date>
    </item>
    <item>
      <title>Re: Un-bonded Pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Un-bonded-Pins/m-p/704228#M28357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bob_walker,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Actually, SWM is defined the according internal block interface to the detail chip pin, PIO0_0 to PIO0_28.&lt;/P&gt;&lt;P&gt;&amp;nbsp; What do you mean:unbonded I/O?&lt;/P&gt;&lt;P&gt;&amp;nbsp; Do you mean? Take an example:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29334iC64BD3B692BD566B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; This pin don't have PIO0_20, but if you use SWM connect the internal block, various block, no external pin, but the internal different block will be connected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; This picture may help you to understand it.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29401iB984230AE50686E6/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Sep 2017 06:05:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Un-bonded-Pins/m-p/704228#M28357</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-09-15T06:05:02Z</dc:date>
    </item>
    <item>
      <title>Re: Un-bonded Pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Un-bonded-Pins/m-p/704229#M28358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;An un-bonded pin is the example you just gave. PIO0_20 does not exist on the package (un-bonded). However, it does exist on the chip. This is the answer I was looking for. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Sep 2017 16:38:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Un-bonded-Pins/m-p/704229#M28358</guid>
      <dc:creator>bob_walker</dc:creator>
      <dc:date>2017-09-15T16:38:33Z</dc:date>
    </item>
  </channel>
</rss>