<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flash memory interfacing LPC1788 does not exit busy state in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-memory-interfacing-LPC1788-does-not-exit-busy-state/m-p/701679#M28240</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a project using LPC1788 micro-controller. I should mention that this micro has external memory controller and the micro interfacing flash using its own controller.&lt;/P&gt;&lt;P&gt;I'm trying to make an external flash memory work, but the problem is after erasing one block, the flash does not exit from the busy state. I use an &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;oscilloscope&lt;/SPAN&gt;&lt;/SPAN&gt; to see the R/B signal and it never returns to its ready state. I have provided some time after the erase operation to create enough time for flash, but it does not work.&lt;/P&gt;&lt;P&gt;I initialized the memory controller's timing registers but I am not definitely sure whether they are correct.&lt;/P&gt;&lt;P&gt;Another issue which may contribute to this problem is that, for every command or every address i provide, my chip select signal changes its state. What I mean is that for every command/address it becomes low and then returns to high. But the diagram in the flash datasheet shows that it should becomes active, just once for the whole operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;every suggestion would be greatly appreciated,&lt;/P&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Oct 2017 11:08:24 GMT</pubDate>
    <dc:creator>erickim</dc:creator>
    <dc:date>2017-10-09T11:08:24Z</dc:date>
    <item>
      <title>Flash memory interfacing LPC1788 does not exit busy state</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-memory-interfacing-LPC1788-does-not-exit-busy-state/m-p/701679#M28240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a project using LPC1788 micro-controller. I should mention that this micro has external memory controller and the micro interfacing flash using its own controller.&lt;/P&gt;&lt;P&gt;I'm trying to make an external flash memory work, but the problem is after erasing one block, the flash does not exit from the busy state. I use an &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;oscilloscope&lt;/SPAN&gt;&lt;/SPAN&gt; to see the R/B signal and it never returns to its ready state. I have provided some time after the erase operation to create enough time for flash, but it does not work.&lt;/P&gt;&lt;P&gt;I initialized the memory controller's timing registers but I am not definitely sure whether they are correct.&lt;/P&gt;&lt;P&gt;Another issue which may contribute to this problem is that, for every command or every address i provide, my chip select signal changes its state. What I mean is that for every command/address it becomes low and then returns to high. But the diagram in the flash datasheet shows that it should becomes active, just once for the whole operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;every suggestion would be greatly appreciated,&lt;/P&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Oct 2017 11:08:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-memory-interfacing-LPC1788-does-not-exit-busy-state/m-p/701679#M28240</guid>
      <dc:creator>erickim</dc:creator>
      <dc:date>2017-10-09T11:08:24Z</dc:date>
    </item>
    <item>
      <title>Re: Flash memory interfacing LPC1788 does not exit busy state</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-memory-interfacing-LPC1788-does-not-exit-busy-state/m-p/701680#M28241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What type of flash are you using? Ire you using the EMC interface? If yes, I would recommend you to use the norflash_prog or nandflash_prog examples that come with LPCopen as reference, these examples show how to use external NOR/NAND Flash using EMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Oct 2017 21:47:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-memory-interfacing-LPC1788-does-not-exit-busy-state/m-p/701680#M28241</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-10-19T21:47:20Z</dc:date>
    </item>
  </channel>
</rss>