<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピック Can fd interface in LPC54000 series MCU is iso version or not?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-fd-interface-in-LPC54000-series-MCU-is-iso-version-or-not/m-p/699287#M28160</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MCAN controller is designed to provide a full&amp;nbsp;implementation of the CAN protocol according to the CAN Specification Version 2.0 part A&amp;nbsp;and to CAN FD Specification V.1.0&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CAN FD Specification V.1.0：&lt;/SPAN&gt;ISO CAN FD or non-ISO CAN FD？&lt;/P&gt;&lt;P&gt;Thank you！&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 09 Sep 2017 03:43:17 GMT</pubDate>
    <dc:creator>chenyandong</dc:creator>
    <dc:date>2017-09-09T03:43:17Z</dc:date>
    <item>
      <title>Can fd interface in LPC54000 series MCU is iso version or not?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-fd-interface-in-LPC54000-series-MCU-is-iso-version-or-not/m-p/699287#M28160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MCAN controller is designed to provide a full&amp;nbsp;implementation of the CAN protocol according to the CAN Specification Version 2.0 part A&amp;nbsp;and to CAN FD Specification V.1.0&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CAN FD Specification V.1.0：&lt;/SPAN&gt;ISO CAN FD or non-ISO CAN FD？&lt;/P&gt;&lt;P&gt;Thank you！&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Sep 2017 03:43:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-fd-interface-in-LPC54000-series-MCU-is-iso-version-or-not/m-p/699287#M28160</guid>
      <dc:creator>chenyandong</dc:creator>
      <dc:date>2017-09-09T03:43:17Z</dc:date>
    </item>
    <item>
      <title>Re:  Can fd interface in LPC54000 series MCU is iso version or not?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-fd-interface-in-LPC54000-series-MCU-is-iso-version-or-not/m-p/699288#M28161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the control register (CCCR) you can select ISO or Non ISO operation. Please check the LPC546xx user manual, Table 713, for more information.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/UM10912.pdf" title="https://www.nxp.com/docs/en/user-guide/UM10912.pdf"&gt;https://www.nxp.com/docs/en/user-guide/UM10912.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/28629i3FBAC3D8BFE14DBE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Soledad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Sep 2017 23:08:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-fd-interface-in-LPC54000-series-MCU-is-iso-version-or-not/m-p/699288#M28161</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-09-12T23:08:32Z</dc:date>
    </item>
  </channel>
</rss>