<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Can't progrm or debug anymore SWD</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-progrm-or-debug-anymore-SWD/m-p/698782#M28116</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the below link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389040"&gt;ISP Reset over debug&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Aug 2017 16:07:57 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2017-08-15T16:07:57Z</dc:date>
    <item>
      <title>Can't progrm or debug anymore SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-progrm-or-debug-anymore-SWD/m-p/698780#M28114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a board with SWD connecction, which works fine until I add a single line to the source&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Chip_Clock_SetSystemPLLSource(SYSCTL_PLLCLKSRC_SYSOSC);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I'm not able to attach the GDB-Server ("CPU not connected") nor with my stand alone programming tool (J-Flash).&lt;/P&gt;&lt;P&gt;I tried it with different&amp;nbsp;reset strategies and I can verify different signals on the reset line, but still the same, it's not possible to connect to the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, it's not a problem of a single board, I tried the same with &amp;nbsp;two more boards with the same result.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Aug 2017 06:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-progrm-or-debug-anymore-SWD/m-p/698780#M28114</guid>
      <dc:creator>xirxe</dc:creator>
      <dc:date>2017-08-15T06:33:48Z</dc:date>
    </item>
    <item>
      <title>Re: Can't progrm or debug anymore SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-progrm-or-debug-anymore-SWD/m-p/698781#M28115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try to get into the ISP programming mode via pin 12 It should work (I think).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Aug 2017 13:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-progrm-or-debug-anymore-SWD/m-p/698781#M28115</guid>
      <dc:creator>vojtechhavlicek</dc:creator>
      <dc:date>2017-08-15T13:34:09Z</dc:date>
    </item>
    <item>
      <title>Re: Can't progrm or debug anymore SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-progrm-or-debug-anymore-SWD/m-p/698782#M28116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the below link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389040"&gt;ISP Reset over debug&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Aug 2017 16:07:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-progrm-or-debug-anymore-SWD/m-p/698782#M28116</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-08-15T16:07:57Z</dc:date>
    </item>
  </channel>
</rss>