<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: hello，when  using the LPCXpersso54608 Rev B（OM13092）board ,I have got some problems. the SDK downloaded from the NXP is“SDK_2.2_LPC54608J512” 。the dirver examples---SD card interrupt demo，in  the source code，Fsl_sd.c in the SD_Init ()   set BUS_WIDTH  in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/hello-when-using-the-LPCXpersso54608-Rev-B-OM13092-board-I-have/m-p/692820#M27924</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV style="color: #000000; background-color: #ffffff; font-size: 14px;"&gt;Hi &amp;nbsp;Carlos，&lt;/DIV&gt;&lt;DIV style="color: #000000; background-color: #ffffff; font-size: 14px;"&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Thank you very much for your reply.The problem I mentioned maybe has been solved.I think it's the SD card compatibility problem.When I do the examples, I used the TF card, and then use a adapter &amp;nbsp;into the SD card. My cards are Sandisk, 16G, Class4, and Sandisk 32G, Class 10. These cards can not &amp;nbsp;be written or read. But I use a standard SD card (without a adapter), SanDisk, 16G, class4 can read and write, do not change any code.&lt;/DIV&gt;&lt;DIV style="color: #000000; background-color: #ffffff; font-size: 14px;"&gt;&lt;DIV&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I've contacted your agent's FAE, and they've had this problem，too. They're working on it, and &amp;nbsp;will &amp;nbsp;give me new code soon.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Also, in which document do you refer to the "7.4 SDIF issue"? Can you send me the document.&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Aug 2017 06:30:14 GMT</pubDate>
    <dc:creator>zhixiangzeng</dc:creator>
    <dc:date>2017-08-07T06:30:14Z</dc:date>
    <item>
      <title>hello，when  using the LPCXpersso54608 Rev B（OM13092）board ,I have got some problems. the SDK downloaded from the NXP is“SDK_2.2_LPC54608J512” 。the dirver examples---SD card interrupt demo，in  the source code，Fsl_sd.c in the SD_Init ()   set BUS_WIDTH is 1</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/hello-when-using-the-LPCXpersso54608-Rev-B-OM13092-board-I-have/m-p/692818#M27922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello，when &amp;nbsp;using the LPCXpersso54608 Rev B（OM13092）board ,I have got some problems. the SDK downloaded from the NXP is“SDK_2.2_LPC54608J512” 。First，the dirver examples---SD card interrupt demo，in &amp;nbsp;the source code， in the SD_Init () of &amp;nbsp;the file Fsl_sd.c &amp;nbsp;，set BUS_WIDTH is 1 bit, the download firmware &amp;nbsp; after compiled &amp;nbsp;，the board can not run.According to the schematic, SD card data should be 4 bits, I changed to 4 bits, the program is running, but still reported wrong "SD, card, init, failed..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2017 02:13:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/hello-when-using-the-LPCXpersso54608-Rev-B-OM13092-board-I-have/m-p/692818#M27922</guid>
      <dc:creator>zhixiangzeng</dc:creator>
      <dc:date>2017-08-03T02:13:10Z</dc:date>
    </item>
    <item>
      <title>Re: hello，when  using the LPCXpersso54608 Rev B（OM13092）board ,I have got some problems. the SDK downloaded from the NXP is“SDK_2.2_LPC54608J512” 。the dirver examples---SD card interrupt demo，in  the source code，Fsl_sd.c in the SD_Init ()   set BUS_WIDTH</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/hello-when-using-the-LPCXpersso54608-Rev-B-OM13092-board-I-have/m-p/692819#M27923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi zhixiang zeng,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’m using the same software version and board revision:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SDK_2.2_LPCXpresso54608 and LPCXpersso54608 Rev B OM13092.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The unmodified example works in 4-bit mode. At the beginning the SD card comes up by default in 1-bit SD mode, but then it is changed into 4-bit mode after startup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried using a different SD card?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2017 17:50:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/hello-when-using-the-LPCXpersso54608-Rev-B-OM13092-board-I-have/m-p/692819#M27923</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-08-03T17:50:49Z</dc:date>
    </item>
    <item>
      <title>Re: hello，when  using the LPCXpersso54608 Rev B（OM13092）board ,I have got some problems. the SDK downloaded from the NXP is“SDK_2.2_LPC54608J512” 。the dirver examples---SD card interrupt demo，in  the source code，Fsl_sd.c in the SD_Init ()   set BUS_WIDTH</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/hello-when-using-the-LPCXpersso54608-Rev-B-OM13092-board-I-have/m-p/692820#M27924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV style="color: #000000; background-color: #ffffff; font-size: 14px;"&gt;Hi &amp;nbsp;Carlos，&lt;/DIV&gt;&lt;DIV style="color: #000000; background-color: #ffffff; font-size: 14px;"&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Thank you very much for your reply.The problem I mentioned maybe has been solved.I think it's the SD card compatibility problem.When I do the examples, I used the TF card, and then use a adapter &amp;nbsp;into the SD card. My cards are Sandisk, 16G, Class4, and Sandisk 32G, Class 10. These cards can not &amp;nbsp;be written or read. But I use a standard SD card (without a adapter), SanDisk, 16G, class4 can read and write, do not change any code.&lt;/DIV&gt;&lt;DIV style="color: #000000; background-color: #ffffff; font-size: 14px;"&gt;&lt;DIV&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I've contacted your agent's FAE, and they've had this problem，too. They're working on it, and &amp;nbsp;will &amp;nbsp;give me new code soon.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Also, in which document do you refer to the "7.4 SDIF issue"? Can you send me the document.&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Aug 2017 06:30:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/hello-when-using-the-LPCXpersso54608-Rev-B-OM13092-board-I-have/m-p/692820#M27924</guid>
      <dc:creator>zhixiangzeng</dc:creator>
      <dc:date>2017-08-07T06:30:14Z</dc:date>
    </item>
  </channel>
</rss>