<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Currently using LPC82x, but need to also use Linux in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Currently-using-LPC82x-but-need-to-also-use-Linux/m-p/692178#M27911</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Apologies, as I am not technical.&lt;/P&gt;&lt;P&gt;We have some code running on the LPC82X. However we now need to run a Linux processor. Is there a product we can use where we can port the existing code onto the upgraded processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jeremy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 May 2017 11:39:47 GMT</pubDate>
    <dc:creator>jeremyprice</dc:creator>
    <dc:date>2017-05-25T11:39:47Z</dc:date>
    <item>
      <title>Currently using LPC82x, but need to also use Linux</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Currently-using-LPC82x-but-need-to-also-use-Linux/m-p/692178#M27911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Apologies, as I am not technical.&lt;/P&gt;&lt;P&gt;We have some code running on the LPC82X. However we now need to run a Linux processor. Is there a product we can use where we can port the existing code onto the upgraded processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jeremy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 May 2017 11:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Currently-using-LPC82x-but-need-to-also-use-Linux/m-p/692178#M27911</guid>
      <dc:creator>jeremyprice</dc:creator>
      <dc:date>2017-05-25T11:39:47Z</dc:date>
    </item>
    <item>
      <title>Re: Currently using LPC82x, but need to also use Linux</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Currently-using-LPC82x-but-need-to-also-use-Linux/m-p/692179#M27912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please continue the follow up in this thread: &lt;A href="https://community.nxp.com/thread/452017"&gt;Advice on upgrade from LPC82x to Linux based processor&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Soledad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jun 2017 15:42:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Currently-using-LPC82x-but-need-to-also-use-Linux/m-p/692179#M27912</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-06-15T15:42:40Z</dc:date>
    </item>
  </channel>
</rss>