<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックAdvice on upgrade from LPC82x to Linux based processor</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Advice-on-upgrade-from-LPC82x-to-Linux-based-processor/m-p/692146#M27897</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need some help on deciding on a processor, and apologise if I sound ignorant as I am not technical.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We run a GPS pet tracking service. We have some software which is currently running on the&amp;nbsp;LPC82x processor. However we would also like to use some other software which currently runs on Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a processor which will run Linux, and at the same time we can port the existing code across without having to make too many changes?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jeremy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 May 2017 11:30:48 GMT</pubDate>
    <dc:creator>jeremyprice</dc:creator>
    <dc:date>2017-05-25T11:30:48Z</dc:date>
    <item>
      <title>Advice on upgrade from LPC82x to Linux based processor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Advice-on-upgrade-from-LPC82x-to-Linux-based-processor/m-p/692146#M27897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need some help on deciding on a processor, and apologise if I sound ignorant as I am not technical.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We run a GPS pet tracking service. We have some software which is currently running on the&amp;nbsp;LPC82x processor. However we would also like to use some other software which currently runs on Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a processor which will run Linux, and at the same time we can port the existing code across without having to make too many changes?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jeremy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 May 2017 11:30:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Advice-on-upgrade-from-LPC82x-to-Linux-based-processor/m-p/692146#M27897</guid>
      <dc:creator>jeremyprice</dc:creator>
      <dc:date>2017-05-25T11:30:48Z</dc:date>
    </item>
    <item>
      <title>Re: Advice on upgrade from LPC82x to Linux based processor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Advice-on-upgrade-from-LPC82x-to-Linux-based-processor/m-p/692147#M27898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A processor capable of running Linux is very different to an LPC8xx MCU. Apart from other things, below, typically a system running Linux will be physically larger than an MCU-based system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is highly unlikely that you will find something that allows you to run your LPC8xx code unchanged as this code is going to be&amp;nbsp;accessing the peripherals directly and this is not normally possible in Linux (you access peripherals through drivers, but this&amp;nbsp;can make the coding much simpler). Also your code would probably run as a task (or tasks) under Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Next, what is the structure of the code. Is it just a simple loop, does it use interrupts, is it using an RTOS etc? Does it have hard real-time requirements (hard real-time is not normally possible in standard Linux)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What peripherals and other features of the LPC8xx are you using/are required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you considered attaching your existing LPC8xx design to a Linux system, perhaps using a UART, SPI, USB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Without know your exact requirements it is difficult to give a definitive answer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jun 2017 15:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Advice-on-upgrade-from-LPC82x-to-Linux-based-processor/m-p/692147#M27898</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2017-06-15T15:33:27Z</dc:date>
    </item>
  </channel>
</rss>