<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 EEPROM write endurance</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/EEPROM-write-endurance/m-p/691793#M27879</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have question about LPC11U24 on-chip EEPROM endurance. Value of parameter is per byte, or per 64B page?&lt;/P&gt;&lt;P&gt;When I wrote one byte to adress 0x0000, I shorted life for next 63 bytes in page, or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vaclav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Jul 2017 08:01:45 GMT</pubDate>
    <dc:creator>vaclavrojik</dc:creator>
    <dc:date>2017-07-11T08:01:45Z</dc:date>
    <item>
      <title>EEPROM write endurance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/EEPROM-write-endurance/m-p/691793#M27879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have question about LPC11U24 on-chip EEPROM endurance. Value of parameter is per byte, or per 64B page?&lt;/P&gt;&lt;P&gt;When I wrote one byte to adress 0x0000, I shorted life for next 63 bytes in page, or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vaclav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 08:01:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/EEPROM-write-endurance/m-p/691793#M27879</guid>
      <dc:creator>vaclavrojik</dc:creator>
      <dc:date>2017-07-11T08:01:45Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM write endurance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/EEPROM-write-endurance/m-p/691794#M27880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When a single byte is programmed, the energy from the charge pump is concentrated on that one byte. If a page write is used, that energy is dissipated over more bytes, so cell wear is decreased.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 15:33:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/EEPROM-write-endurance/m-p/691794#M27880</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-07-11T15:33:11Z</dc:date>
    </item>
  </channel>
</rss>