<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1549 RTC goes forward 5-6 sec per hour in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-RTC-goes-forward-5-6-sec-per-hour/m-p/688737#M27790</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have already posted this message in another thread several days ago, but I got no answer. This is why I create this&amp;nbsp;new (however redundant) entry...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the RTC of an LPC1549 and the clock goes forward several seconds per hour&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have 5&amp;nbsp;boards and each of them has got the problem:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My application:&lt;/P&gt;&lt;P&gt;Chip: LPC1549JBD48&lt;/P&gt;&lt;P&gt;Identification: ZSD14372A (Production Year 2014 / Week 37 - Silicon revision A)&lt;/P&gt;&lt;P&gt;I am using a 32 KHz cylindrical Xtal with 22 pf capacitors.&lt;/P&gt;&lt;P&gt;Supply: all supplies are clean 3.3 V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RTC oscillator frequency is routed to an I/O port thanks to the CLKOUT feature. My frequency meter indicates 32767,84 Hz - This is a -6 ppm error, yielding a -4 seconds error per WEEK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The counter is used in basic SECONDS mode, without interrupt. I read its value once per second and I send it to my console. After a while, I see the RTC clock going forward several seconds per hour.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Errata sheet LPC15XX 2.2 - 17 february 2017 says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;3.5 RTC.1: Real Time Clock (RTC) does not work reliably. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Introduction: &lt;/STRONG&gt;&lt;STRONG&gt;The RTC is a set of counters for measuring time when system power is on, and optionally when it is off. The RTC is clocked by a separate 32 kHz oscillator that produces a 1 Hz internal time reference. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Problem: &lt;/STRONG&gt;&lt;STRONG&gt;The RTC COUNT should increment by one in one second. With the problem, the RTC COUNT might increment by more than one within one second, causing inaccurate time counting. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Work-around: None. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - Assuming there is no direct work-around for this issue - Is there a known, simple and reliable way to use the on board 12 MHz Xtal oscillator to achieve coherence checking and remove the redundant pulses whenever they appear ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2 - has this issue been fixed in new silicon. Are these new devices available ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Michel Kuenemann&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Jul 2017 07:55:55 GMT</pubDate>
    <dc:creator>michelkuenemann</dc:creator>
    <dc:date>2017-07-31T07:55:55Z</dc:date>
    <item>
      <title>LPC1549 RTC goes forward 5-6 sec per hour</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-RTC-goes-forward-5-6-sec-per-hour/m-p/688737#M27790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have already posted this message in another thread several days ago, but I got no answer. This is why I create this&amp;nbsp;new (however redundant) entry...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the RTC of an LPC1549 and the clock goes forward several seconds per hour&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have 5&amp;nbsp;boards and each of them has got the problem:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My application:&lt;/P&gt;&lt;P&gt;Chip: LPC1549JBD48&lt;/P&gt;&lt;P&gt;Identification: ZSD14372A (Production Year 2014 / Week 37 - Silicon revision A)&lt;/P&gt;&lt;P&gt;I am using a 32 KHz cylindrical Xtal with 22 pf capacitors.&lt;/P&gt;&lt;P&gt;Supply: all supplies are clean 3.3 V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RTC oscillator frequency is routed to an I/O port thanks to the CLKOUT feature. My frequency meter indicates 32767,84 Hz - This is a -6 ppm error, yielding a -4 seconds error per WEEK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The counter is used in basic SECONDS mode, without interrupt. I read its value once per second and I send it to my console. After a while, I see the RTC clock going forward several seconds per hour.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Errata sheet LPC15XX 2.2 - 17 february 2017 says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;3.5 RTC.1: Real Time Clock (RTC) does not work reliably. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Introduction: &lt;/STRONG&gt;&lt;STRONG&gt;The RTC is a set of counters for measuring time when system power is on, and optionally when it is off. The RTC is clocked by a separate 32 kHz oscillator that produces a 1 Hz internal time reference. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Problem: &lt;/STRONG&gt;&lt;STRONG&gt;The RTC COUNT should increment by one in one second. With the problem, the RTC COUNT might increment by more than one within one second, causing inaccurate time counting. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Work-around: None. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - Assuming there is no direct work-around for this issue - Is there a known, simple and reliable way to use the on board 12 MHz Xtal oscillator to achieve coherence checking and remove the redundant pulses whenever they appear ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2 - has this issue been fixed in new silicon. Are these new devices available ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Michel Kuenemann&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2017 07:55:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-RTC-goes-forward-5-6-sec-per-hour/m-p/688737#M27790</guid>
      <dc:creator>michelkuenemann</dc:creator>
      <dc:date>2017-07-31T07:55:55Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1549 RTC goes forward 5-6 sec per hour</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-RTC-goes-forward-5-6-sec-per-hour/m-p/688738#M27791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Answering your questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Unfortunately we and still don't have a workaround for this design defect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We still don't have information for next generation of LPC15xx.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Aug 2017 14:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-RTC-goes-forward-5-6-sec-per-hour/m-p/688738#M27791</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-08-02T14:14:57Z</dc:date>
    </item>
  </channel>
</rss>