<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Core / Peripheral States after wakeup from low power mode in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Core-Peripheral-States-after-wakeup-from-low-power-mode/m-p/688380#M27754</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="297396" data-username="simonwyss" href="https://community.nxp.com/people/simonwyss"&gt;Simon Wyss&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;1) when I switch to the RTC (32kHz) bevor going to sleep, deep-sleep or power-down, what happens on wakeup?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I think the MCU will resume execute after wake up events happen.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Aug 2017 05:35:48 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2017-08-01T05:35:48Z</dc:date>
    <item>
      <title>Core / Peripheral States after wakeup from low power mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Core-Peripheral-States-after-wakeup-from-low-power-mode/m-p/688379#M27753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which peripherals are powered after different low power states?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found some information in the application note AN11611 and the user-manual UM10850 but I don't know if the RTC is always started after reset from sleep, deep-sleep or power-down mode?&lt;BR /&gt;If I use only the IRC as clock, I think the IRC has to start after the sleep, deep-sleep or power-down mode. Because ther is no other clock available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when I switch to the RTC (32kHz) bevor going to sleep, deep-sleep or power-down, what happens on wakeup?&lt;BR /&gt;Is the IRC automatically started? Is the main-clock-source automatically switched to the IRC clock?&lt;BR /&gt;If not, I would have to switch the main-clock-source manually to IRC (with the 32kHz Clock, using 32us for each CPU cycle)&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Thank you in advance for your help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4018iA447660C809606EC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There seems to be an error in the AN11611 on page 5: The IRC is shutdown in Deep-Sleep according to the user-manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4063i6EB3E1E55B0C0188/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2017 07:11:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Core-Peripheral-States-after-wakeup-from-low-power-mode/m-p/688379#M27753</guid>
      <dc:creator>simonwyss</dc:creator>
      <dc:date>2017-07-31T07:11:26Z</dc:date>
    </item>
    <item>
      <title>Re: Core / Peripheral States after wakeup from low power mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Core-Peripheral-States-after-wakeup-from-low-power-mode/m-p/688380#M27754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="297396" data-username="simonwyss" href="https://community.nxp.com/people/simonwyss"&gt;Simon Wyss&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;1) when I switch to the RTC (32kHz) bevor going to sleep, deep-sleep or power-down, what happens on wakeup?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I think the MCU will resume execute after wake up events happen.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Aug 2017 05:35:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Core-Peripheral-States-after-wakeup-from-low-power-mode/m-p/688380#M27754</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2017-08-01T05:35:48Z</dc:date>
    </item>
    <item>
      <title>Re: Core / Peripheral States after wakeup from low power mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Core-Peripheral-States-after-wakeup-from-low-power-mode/m-p/688381#M27755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jeremyzhou"&gt;jeremyzhou&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;Thank you for your reply!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Which is&amp;nbsp;the main-clock-source after wakeup?&amp;nbsp;&lt;/P&gt;&lt;P&gt;- RTC (32kHz)&lt;/P&gt;&lt;P&gt;- IRC (12MHz)&lt;BR /&gt;&lt;BR /&gt;2) Is the IRC always powered up after wakeup?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Aug 2017 07:31:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Core-Peripheral-States-after-wakeup-from-low-power-mode/m-p/688381#M27755</guid>
      <dc:creator>simonwyss</dc:creator>
      <dc:date>2017-08-01T07:31:01Z</dc:date>
    </item>
    <item>
      <title>Re: Core / Peripheral States after wakeup from low power mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Core-Peripheral-States-after-wakeup-from-low-power-mode/m-p/688382#M27756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="297396" data-username="simonwyss" href="https://community.nxp.com/people/simonwyss"&gt;Simon Wyss&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;1) Which is&amp;nbsp;the main-clock-source after wakeup?&amp;nbsp;&lt;/P&gt;&lt;P&gt;- RTC (32kHz)&lt;/P&gt;&lt;P&gt;- IRC (12MHz)&lt;/P&gt;&lt;P&gt;Depend on the previous option configured, the MCU will resume execute with the original clock source after wake up.&lt;/P&gt;&lt;P&gt;Please you can have a try.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Aug 2017 08:54:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Core-Peripheral-States-after-wakeup-from-low-power-mode/m-p/688382#M27756</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2017-08-01T08:54:49Z</dc:date>
    </item>
  </channel>
</rss>