<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC1549 LPCXpresso board - Problem when connected with a serial terminal in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-LPCXpresso-board-Problem-when-connected-with-a-serial/m-p/688235#M27747</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;At the moment, the probe firmware is being soft loaded when you start a debug session by the IDE. For what you are trying to do, you need&amp;nbsp;&amp;nbsp;pre-program the debug probe firmware into the onboard LPC-Link2's flash memory, using LPCScrypt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more details see:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/thread/389045"&gt;LPC-Link2 Debug Probe firmware programming&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;&lt;A class="link-titled" href="http://www.nxp.com/LPCScrypt" title="http://www.nxp.com/LPCScrypt"&gt;LPCScrypt v1.8.2|NXP&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Jul 2017 21:28:40 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2017-07-07T21:28:40Z</dc:date>
    <item>
      <title>LPC1549 LPCXpresso board - Problem when connected with a serial terminal</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-LPCXpresso-board-Problem-when-connected-with-a-serial/m-p/688234#M27746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV&gt;I am using LPCXpresso1549 demo board. I connect it to my PC with the LPCXpresso IDE&amp;nbsp;and I can download and debug my code. I&amp;nbsp;need to use a serial terminal (Tera Term) to display debugging messages. But I can use this ONLY after I download my code into the board through LPCXpresso IDE, while the board is still connected. After downloading, when I give the command "New Connection" from&amp;nbsp;the serial terminal (Tera Term),&amp;nbsp;it will appear: "COM4: LPC - LinkII UCom Port (COM4)" as a choice&amp;nbsp;and I can connect my board to the serial terminal. So this is OK.&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;But, if I disconnect the board from the PC (disconnecting the USB cable), and then connect it again, I cannot display anything on the serial terminal. When I&amp;nbsp;give the command "New Connection" from the serial terminal (Tera Term), it does not show the Port # where the LPCXpresso1549 demo board is plugged in. So I cannot choose the board for connecting to the serial terminal.&lt;/DIV&gt;&lt;DIV&gt;Also in the Device Manager the board appears now under&amp;nbsp;"LPCDevice" as "LPC based USB device", whereas in the above situation after downloading, it appeared under&amp;nbsp;"Ports (COM &amp;amp; LPT)"&amp;nbsp;as "LPC - LinkII UCom Port (COM4)".&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I need to use this board in a testing environment where there is not a computer having LPCXpresso IDE&amp;nbsp;installed. So I need to download my code into the board through LPCXpresso IDE on my PC, take the board and use it with a serial terminal (Tera Term) on another computer in that testing environment, but I cannot use it because the board is not recognized by the serial terminal on that computer.&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I would really appreciate any help!&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Thank you,&lt;/DIV&gt;&lt;DIV&gt;Doini&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 19:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-LPCXpresso-board-Problem-when-connected-with-a-serial/m-p/688234#M27746</guid>
      <dc:creator>doini</dc:creator>
      <dc:date>2017-07-07T19:26:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1549 LPCXpresso board - Problem when connected with a serial terminal</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-LPCXpresso-board-Problem-when-connected-with-a-serial/m-p/688235#M27747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;At the moment, the probe firmware is being soft loaded when you start a debug session by the IDE. For what you are trying to do, you need&amp;nbsp;&amp;nbsp;pre-program the debug probe firmware into the onboard LPC-Link2's flash memory, using LPCScrypt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more details see:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/thread/389045"&gt;LPC-Link2 Debug Probe firmware programming&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;&lt;A class="link-titled" href="http://www.nxp.com/LPCScrypt" title="http://www.nxp.com/LPCScrypt"&gt;LPCScrypt v1.8.2|NXP&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 21:28:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-LPCXpresso-board-Problem-when-connected-with-a-serial/m-p/688235#M27747</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-07-07T21:28:40Z</dc:date>
    </item>
  </channel>
</rss>