<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC2294 External Flash Read and Write</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2294-External-Flash-Read-and-Write/m-p/684577#M27572</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;UL&gt;&lt;LI&gt;i use software "JFlash" to program on external flash, but there is an error "programming failed @address 0x80000000 ". there is nothing wrong when erasing and reading back, but the pin WE is always high while programming. could you tell me the reason？ The picture of JFLASH is as follow:&lt;/LI&gt;&lt;LI&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20401i1EF95BF5FAD8A033/image-size/large?v=v2&amp;amp;px=999" title="微信图片_20170613174200.jpg" alt="微信图片_20170613174200.jpg" /&gt;&lt;/span&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jun 2017 09:48:28 GMT</pubDate>
    <dc:creator>1263906294</dc:creator>
    <dc:date>2017-06-13T09:48:28Z</dc:date>
    <item>
      <title>LPC2294 External Flash Read and Write</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2294-External-Flash-Read-and-Write/m-p/684577#M27572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;UL&gt;&lt;LI&gt;i use software "JFlash" to program on external flash, but there is an error "programming failed @address 0x80000000 ". there is nothing wrong when erasing and reading back, but the pin WE is always high while programming. could you tell me the reason？ The picture of JFLASH is as follow:&lt;/LI&gt;&lt;LI&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20401i1EF95BF5FAD8A033/image-size/large?v=v2&amp;amp;px=999" title="微信图片_20170613174200.jpg" alt="微信图片_20170613174200.jpg" /&gt;&lt;/span&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 09:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2294-External-Flash-Read-and-Write/m-p/684577#M27572</guid>
      <dc:creator>1263906294</dc:creator>
      <dc:date>2017-06-13T09:48:28Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2294 External Flash Read and Write</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2294-External-Flash-Read-and-Write/m-p/684578#M27573</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Most of the times, it would be required to generate a proper configuration file according to the used external memory. You could take a look at the following links, that may provide useful related information, depending of the hardware, IDE and debug tool:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.lpcware.com/content/forum/help-j-link-program"&gt;https://www.lpcware.com/content/forum/help-j-link-program&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.embeddedrelated.com/showthread/lpc2000/8706-1.php"&gt;https://www.embeddedrelated.com/showthread/lpc2000/8706-1.php&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.keil.com/forum/6027/"&gt;http://www.keil.com/forum/6027/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forum.segger.com/index.php?page=Thread&amp;amp;threadID=20"&gt;http://forum.segger.com/index.php?page=Thread&amp;amp;threadID=20&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.embeddedrelated.com/showthread/lpc2000/35484-1.php"&gt;https://www.embeddedrelated.com/showthread/lpc2000/35484-1.php&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.lpcware.com/content/forum/need-help-programming-external-flash-lpc-link2-board"&gt;https://www.lpcware.com/content/forum/need-help-programming-external-flash-lpc-link2-board&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Jun 2017 00:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2294-External-Flash-Read-and-Write/m-p/684578#M27573</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2017-06-17T00:29:04Z</dc:date>
    </item>
  </channel>
</rss>