<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC1313 toggling GPIO pins</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1313-toggling-GPIO-pins/m-p/679798#M27331</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was able to find a workaround. The problem is seen when I use the&amp;nbsp;Chip_GPIO_SetDir function to set the pin directions instead of&amp;nbsp;Chip_GPIO_SetPinDIROutput. The&amp;nbsp;&lt;SPAN&gt;Chip_GPIO_SetDir function doesn't seem to set the direction bits for some pins properly. However, I couldn't find the reason for the same.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks and Regards.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 May 2017 03:56:22 GMT</pubDate>
    <dc:creator>prachipanse</dc:creator>
    <dc:date>2017-05-16T03:56:22Z</dc:date>
    <item>
      <title>LPC1313 toggling GPIO pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1313-toggling-GPIO-pins/m-p/679797#M27330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using the LPC1313FBD48/01 controller to toggle some LEDs. I am using the LPCOpen library.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I observed in the GPIO registers that some GPIO outputs are not getting set (IOCON_PIO0_11 and IOCON_PIO1_10). Using the same procedure I am able to toggle the pin IOCON_PIO1_1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest me what may be the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 May 2017 11:15:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1313-toggling-GPIO-pins/m-p/679797#M27330</guid>
      <dc:creator>prachipanse</dc:creator>
      <dc:date>2017-05-15T11:15:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1313 toggling GPIO pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1313-toggling-GPIO-pins/m-p/679798#M27331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was able to find a workaround. The problem is seen when I use the&amp;nbsp;Chip_GPIO_SetDir function to set the pin directions instead of&amp;nbsp;Chip_GPIO_SetPinDIROutput. The&amp;nbsp;&lt;SPAN&gt;Chip_GPIO_SetDir function doesn't seem to set the direction bits for some pins properly. However, I couldn't find the reason for the same.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks and Regards.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 03:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1313-toggling-GPIO-pins/m-p/679798#M27331</guid>
      <dc:creator>prachipanse</dc:creator>
      <dc:date>2017-05-16T03:56:22Z</dc:date>
    </item>
  </channel>
</rss>