<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Slave I2C1 Test with master I2C0</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Slave-I2C1-Test-with-master-I2C0/m-p/678069#M27247</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am implement the I2C slave function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MCB1857 EVA&amp;nbsp;board, I want to confirm if I can set I2C0 to master and set I2C1 to slave mode,&lt;/P&gt;&lt;P&gt;and connect each SCL and SDA to transmit data(i2c0 sends to i2c1)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jun 2017 09:34:31 GMT</pubDate>
    <dc:creator>kensu</dc:creator>
    <dc:date>2017-06-07T09:34:31Z</dc:date>
    <item>
      <title>Slave I2C1 Test with master I2C0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Slave-I2C1-Test-with-master-I2C0/m-p/678069#M27247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am implement the I2C slave function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MCB1857 EVA&amp;nbsp;board, I want to confirm if I can set I2C0 to master and set I2C1 to slave mode,&lt;/P&gt;&lt;P&gt;and connect each SCL and SDA to transmit data(i2c0 sends to i2c1)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 09:34:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Slave-I2C1-Test-with-master-I2C0/m-p/678069#M27247</guid>
      <dc:creator>kensu</dc:creator>
      <dc:date>2017-06-07T09:34:31Z</dc:date>
    </item>
    <item>
      <title>Re: Slave I2C1 Test with master I2C0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Slave-I2C1-Test-with-master-I2C0/m-p/678070#M27248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ken Su,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Of course you can!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I2C0 and I2C1 are the independent module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You can use any one as master, and another one as slave.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Just do it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 07:08:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Slave-I2C1-Test-with-master-I2C0/m-p/678070#M27248</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-06-08T07:08:33Z</dc:date>
    </item>
  </channel>
</rss>