<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1788FBD208 Pin compatible</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788FBD208-Pin-compatible/m-p/676556#M27144</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand NXP just released LPC546xx. I saw specification of this part can be upgraded for LPC1788FBD208. Does LPC546xx have part number which is pin to pin compatible with LPC1788FBD208?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wittawas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Jun 2017 07:36:57 GMT</pubDate>
    <dc:creator>Childe</dc:creator>
    <dc:date>2017-06-06T07:36:57Z</dc:date>
    <item>
      <title>LPC1788FBD208 Pin compatible</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788FBD208-Pin-compatible/m-p/676556#M27144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand NXP just released LPC546xx. I saw specification of this part can be upgraded for LPC1788FBD208. Does LPC546xx have part number which is pin to pin compatible with LPC1788FBD208?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wittawas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jun 2017 07:36:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788FBD208-Pin-compatible/m-p/676556#M27144</guid>
      <dc:creator>Childe</dc:creator>
      <dc:date>2017-06-06T07:36:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788FBD208 Pin compatible</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788FBD208-Pin-compatible/m-p/676557#M27145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wittawas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LPC546xx does not have a pin to pin compatible part number with the LPC1788FBD208 but the LPC408x is pin compatible with LPC1778x with enhancements in the core and advanced peripherals. The following application note highlights some of the differences between these two families and provides guidance when switching from the LPC178x based hardware/software to the LPC408x systems:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/documents/application_note/AN11335.zip?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="http://cache.nxp.com/documents/application_note/AN11335.zip?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;http://cache.nxp.com/documents/application_note/AN11335.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 16:43:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788FBD208-Pin-compatible/m-p/676557#M27145</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-06-08T16:43:28Z</dc:date>
    </item>
  </channel>
</rss>