<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 maximum output timer lpc4337</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/maximum-output-timer-lpc4337/m-p/674473#M27012</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi I'm working on lpc4337 and I'm trying generate an output with a timer as 10mhz frequency and I just can get approximately 300khz. That's possible?get an output higher as 10mhz??regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 03 Jun 2017 14:25:12 GMT</pubDate>
    <dc:creator>diegotorres</dc:creator>
    <dc:date>2017-06-03T14:25:12Z</dc:date>
    <item>
      <title>maximum output timer lpc4337</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/maximum-output-timer-lpc4337/m-p/674473#M27012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi I'm working on lpc4337 and I'm trying generate an output with a timer as 10mhz frequency and I just can get approximately 300khz. That's possible?get an output higher as 10mhz??regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Jun 2017 14:25:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/maximum-output-timer-lpc4337/m-p/674473#M27012</guid>
      <dc:creator>diegotorres</dc:creator>
      <dc:date>2017-06-03T14:25:12Z</dc:date>
    </item>
    <item>
      <title>Re: maximum output timer lpc4337</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/maximum-output-timer-lpc4337/m-p/674474#M27013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which timer are you using?&lt;/P&gt;&lt;P&gt;Please check the AN11538 application note, this application note is a collection of examples and usage notes for the&lt;BR /&gt;SCTimer/PWM block used in NXP microcontrollers.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/documents/application_note/AN11538.zip" title="http://www.nxp.com/documents/application_note/AN11538.zip"&gt;http://www.nxp.com/documents/application_note/AN11538.zip&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 21:46:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/maximum-output-timer-lpc4337/m-p/674474#M27013</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-06-08T21:46:13Z</dc:date>
    </item>
  </channel>
</rss>