<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What voltage regulators should I use for the LPC11C24? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-voltage-regulators-should-I-use-for-the-LPC11C24/m-p/674349#M27011</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Usually that minimum current is fairly small, a few mA, you could have just an LED to tell the thing is powered up.&lt;/P&gt;&lt;P&gt;I would first guess what your maximum current is, I assume not more than 100 mA, so you can choose a linear regulator with those ratings:&lt;/P&gt;&lt;P&gt;Vin &amp;gt; 12V, Vout 3V3 or 5V, Iout &amp;gt;= 100mA&lt;/P&gt;&lt;P&gt;An additional note on power: for 12V in, 3V out you will dissipate 0,9W at 100 mA. That's relatively a lot, the smallest packages (SOT-23) may not cope with that, check the ones in DPAK, etc. Also, for your PCB, keep a decent copper area and vias to ground plane for heat sinking.&lt;/P&gt;&lt;P&gt;Alternatively, the cooler although pricier way is to have a switching regulator. You can get 90% efficiency but will have to design it, put more components, etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Jul 2017 11:01:29 GMT</pubDate>
    <dc:creator>juanabelaira</dc:creator>
    <dc:date>2017-07-20T11:01:29Z</dc:date>
    <item>
      <title>What voltage regulators should I use for the LPC11C24?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-voltage-regulators-should-I-use-for-the-LPC11C24/m-p/674347#M27009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LPC11C24 needs 3.3V and 5V (for CAN). Could anyone recommend me some stable voltage regulators to use? My input will be 12V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One concern I have is current draw. I noticed that voltage regulators have a minimum current load requirement in order to be stable. After some research, I estimate that I should be drawing from 5-50mA for the 5V regulator (powers CAN transceiver) and around 10mA for the 3.3V &amp;nbsp;regulator (powers microcontroller and a current sensor).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2017 19:38:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-voltage-regulators-should-I-use-for-the-LPC11C24/m-p/674347#M27009</guid>
      <dc:creator>matthewfilibert</dc:creator>
      <dc:date>2017-07-18T19:38:33Z</dc:date>
    </item>
    <item>
      <title>Re: What voltage regulators should I use for the LPC11C24?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-voltage-regulators-should-I-use-for-the-LPC11C24/m-p/674348#M27010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use some schematic file as reference, for example check the below link:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.olimex.com/Products/ARM/NXP/LPC-P11C24/resources/LPC-P11C24_revision_A_sch.pdf" title="https://www.olimex.com/Products/ARM/NXP/LPC-P11C24/resources/LPC-P11C24_revision_A_sch.pdf"&gt;https://www.olimex.com/Products/ARM/NXP/LPC-P11C24/resources/LPC-P11C24_revision_A_sch.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 18:55:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-voltage-regulators-should-I-use-for-the-LPC11C24/m-p/674348#M27010</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-07-19T18:55:13Z</dc:date>
    </item>
    <item>
      <title>Re: What voltage regulators should I use for the LPC11C24?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-voltage-regulators-should-I-use-for-the-LPC11C24/m-p/674349#M27011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Usually that minimum current is fairly small, a few mA, you could have just an LED to tell the thing is powered up.&lt;/P&gt;&lt;P&gt;I would first guess what your maximum current is, I assume not more than 100 mA, so you can choose a linear regulator with those ratings:&lt;/P&gt;&lt;P&gt;Vin &amp;gt; 12V, Vout 3V3 or 5V, Iout &amp;gt;= 100mA&lt;/P&gt;&lt;P&gt;An additional note on power: for 12V in, 3V out you will dissipate 0,9W at 100 mA. That's relatively a lot, the smallest packages (SOT-23) may not cope with that, check the ones in DPAK, etc. Also, for your PCB, keep a decent copper area and vias to ground plane for heat sinking.&lt;/P&gt;&lt;P&gt;Alternatively, the cooler although pricier way is to have a switching regulator. You can get 90% efficiency but will have to design it, put more components, etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 11:01:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-voltage-regulators-should-I-use-for-the-LPC11C24/m-p/674349#M27011</guid>
      <dc:creator>juanabelaira</dc:creator>
      <dc:date>2017-07-20T11:01:29Z</dc:date>
    </item>
  </channel>
</rss>