<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1830/1857  SDRAM as heap</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1830-1857-SDRAM-as-heap/m-p/673980#M26985</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using 1830 and 1857 with MCUXpresso IDE (I convert the LPC sample project to MCUXpresso).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because my application use large memory size and I have external SDRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use SDRAM as heap, but it need to execute SDRAM initial() function in board.c with internal SRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the SDRAM can work as heap correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are some SDRAM as heap article. some is using IAR, some are using other MCU. It seems there are many method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could someone give guild how to make SDRAM as heap and execute the SDRAM initial() code with SRAM.&lt;/P&gt;&lt;P&gt;With MCUXpresso or LPCXpresso, and the MCU is LPC1830/LPC1857.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 May 2017 16:05:07 GMT</pubDate>
    <dc:creator>kensu</dc:creator>
    <dc:date>2017-05-09T16:05:07Z</dc:date>
    <item>
      <title>LPC1830/1857  SDRAM as heap</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1830-1857-SDRAM-as-heap/m-p/673980#M26985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using 1830 and 1857 with MCUXpresso IDE (I convert the LPC sample project to MCUXpresso).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because my application use large memory size and I have external SDRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use SDRAM as heap, but it need to execute SDRAM initial() function in board.c with internal SRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the SDRAM can work as heap correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are some SDRAM as heap article. some is using IAR, some are using other MCU. It seems there are many method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could someone give guild how to make SDRAM as heap and execute the SDRAM initial() code with SRAM.&lt;/P&gt;&lt;P&gt;With MCUXpresso or LPCXpresso, and the MCU is LPC1830/LPC1857.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 May 2017 16:05:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1830-1857-SDRAM-as-heap/m-p/673980#M26985</guid>
      <dc:creator>kensu</dc:creator>
      <dc:date>2017-05-09T16:05:07Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1830/1857  SDRAM as heap</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1830-1857-SDRAM-as-heap/m-p/673981#M26986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the below links:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.lpcware.com/content/forum/allocating-dynamic-memory-external-sdram" title="https://www.lpcware.com/content/forum/allocating-dynamic-memory-external-sdram"&gt;Allocating dynamic memory in External SDRAM | www.LPCware.com&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389026"&gt;Heap allocation/checking in Redlib&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Soledad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 May 2017 21:17:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1830-1857-SDRAM-as-heap/m-p/673981#M26986</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-05-17T21:17:26Z</dc:date>
    </item>
  </channel>
</rss>