<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 uint8_t range of values</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/uint8-t-range-of-values/m-p/673503#M26943</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I use the LPC11C24 development board, the use of uint8_t (unsigned char) type of array. Found it can only be in the value of 0 to 127, in fact it should be 0 to 255. The highest bit can not be used, which is why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Jun 2017 07:38:41 GMT</pubDate>
    <dc:creator>vnv</dc:creator>
    <dc:date>2017-06-02T07:38:41Z</dc:date>
    <item>
      <title>uint8_t range of values</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/uint8-t-range-of-values/m-p/673503#M26943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I use the LPC11C24 development board, the use of uint8_t (unsigned char) type of array. Found it can only be in the value of 0 to 127, in fact it should be 0 to 255. The highest bit can not be used, which is why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 07:38:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/uint8-t-range-of-values/m-p/673503#M26943</guid>
      <dc:creator>vnv</dc:creator>
      <dc:date>2017-06-02T07:38:41Z</dc:date>
    </item>
    <item>
      <title>Re: uint8_t range of values</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/uint8-t-range-of-values/m-p/673504#M26944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Works (correctly) for me. What is your code, and how are you checking your values?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 09:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/uint8-t-range-of-values/m-p/673504#M26944</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2017-06-02T09:35:02Z</dc:date>
    </item>
    <item>
      <title>Re: uint8_t range of values</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/uint8-t-range-of-values/m-p/673505#M26945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi，&lt;/P&gt;&lt;P&gt;My screenshot is as follows:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19615iF0139181AB33C031/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19686i32F05D9B10B02F81/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a program I developed with SPI，Please take a look&amp;nbsp;Tx_Buf[3] ,Tx_Buf[4],&amp;nbsp;Tx_Buf[5] ,Tx_Buf[6] ,The value in memory.&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;The highest bit can not be used.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 10:22:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/uint8-t-range-of-values/m-p/673505#M26945</guid>
      <dc:creator>vnv</dc:creator>
      <dc:date>2017-06-02T10:22:30Z</dc:date>
    </item>
    <item>
      <title>Re: uint8_t range of values</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/uint8-t-range-of-values/m-p/673506#M26946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That is a bug in the display of your IDE, nothing wrong with the code or the values. Complain to your IDE vendor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the output in MCUXpresso&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20066iBAB0C2B9D07F29D5/image-size/large?v=v2&amp;amp;px=999" title="2017-06-02 12.47.31 pm.png" alt="2017-06-02 12.47.31 pm.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20017i38BD3DC5EF732D9B/image-size/large?v=v2&amp;amp;px=999" title="2017-06-02 12.47.43 pm.png" alt="2017-06-02 12.47.43 pm.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 11:49:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/uint8-t-range-of-values/m-p/673506#M26946</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2017-06-02T11:49:33Z</dc:date>
    </item>
  </channel>
</rss>