<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1778 getting corrupt after programming from a ttl port in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-getting-corrupt-after-programming-from-a-ttl-port/m-p/671072#M26836</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using LPC1778 IC as a microcontoller for our design, We fabricated that after 3 years of purchase, Is there any chances of LPC misbehaving/Corrupting&amp;nbsp; if it is not baked properly and mounted on the PCB???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Jul 2017 04:56:37 GMT</pubDate>
    <dc:creator>karthikks</dc:creator>
    <dc:date>2017-07-17T04:56:37Z</dc:date>
    <item>
      <title>LPC1778 getting corrupt after programming from a ttl port</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-getting-corrupt-after-programming-from-a-ttl-port/m-p/671072#M26836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using LPC1778 IC as a microcontoller for our design, We fabricated that after 3 years of purchase, Is there any chances of LPC misbehaving/Corrupting&amp;nbsp; if it is not baked properly and mounted on the PCB???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jul 2017 04:56:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-getting-corrupt-after-programming-from-a-ttl-port/m-p/671072#M26836</guid>
      <dc:creator>karthikks</dc:creator>
      <dc:date>2017-07-17T04:56:37Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 getting corrupt after programming from a ttl port</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-getting-corrupt-after-programming-from-a-ttl-port/m-p/671073#M26837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello KARTHIK KS,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Do you mean you are using the UART ISP to download the code to the LPC1778, but the downloading is failed?&lt;/P&gt;&lt;P&gt;&amp;nbsp; When you use the ISP, do you enter the ISP mode correctly?&lt;/P&gt;&lt;P&gt;&amp;nbsp;A LOW level after reset at pin P2[10] is considered an external hardware request to start the ISP command handler using UART0 pins P0[2] (U0_TXD) and P0[3] (U0_RXD).&lt;/P&gt;&lt;P&gt;&amp;nbsp; Besides, you need to check your TTL, whether the voltage is exceed the LPC1778 max voltage. If the voltage is exceed the max lpc1778 data, it may damages the pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp; When the corrupt happens, do you also use the SWD or the JTAGE interface, and download it by the debugger(for example JLINK)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2017 05:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-getting-corrupt-after-programming-from-a-ttl-port/m-p/671073#M26837</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-07-18T05:58:57Z</dc:date>
    </item>
  </channel>
</rss>