<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC43xx sd/mmc card acquire fails in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sd-mmc-card-acquire-fails/m-p/669947#M26797</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPC43S57 MCU, using SD/MMC driver (CIU). SD_CMD signal phase is opposite that needed by my card. Is there any way to change the 'phase' of the SD_CMD/SD_DATn signals so they are valid on the rising edge of SD_CLK instead of being valid on the falling edge of SD_CLK during card acquire? (CMD0, CMD1, CMD2).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running the sd/mmc example code from LPC43xx examples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Windows, Linux, and OSX hosts all use 'phase 0', data valid on rising edge of SD_CLK. Why is the LPC43S57 SD/MMC host opposite?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Jun 2017 15:49:10 GMT</pubDate>
    <dc:creator>rickrigby</dc:creator>
    <dc:date>2017-06-22T15:49:10Z</dc:date>
    <item>
      <title>LPC43xx sd/mmc card acquire fails</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sd-mmc-card-acquire-fails/m-p/669947#M26797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPC43S57 MCU, using SD/MMC driver (CIU). SD_CMD signal phase is opposite that needed by my card. Is there any way to change the 'phase' of the SD_CMD/SD_DATn signals so they are valid on the rising edge of SD_CLK instead of being valid on the falling edge of SD_CLK during card acquire? (CMD0, CMD1, CMD2).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running the sd/mmc example code from LPC43xx examples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Windows, Linux, and OSX hosts all use 'phase 0', data valid on rising edge of SD_CLK. Why is the LPC43S57 SD/MMC host opposite?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jun 2017 15:49:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sd-mmc-card-acquire-fails/m-p/669947#M26797</guid>
      <dc:creator>rickrigby</dc:creator>
      <dc:date>2017-06-22T15:49:10Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx sd/mmc card acquire fails</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sd-mmc-card-acquire-fails/m-p/669948#M26798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see some discussion on this but didn't try myself:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.lpcware.com/zh-hans/node/1110550"&gt;https://www.lpcware.com/zh-hans/node/1110550&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jun 2017 17:20:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-sd-mmc-card-acquire-fails/m-p/669948#M26798</guid>
      <dc:creator>Dezheng_Tang</dc:creator>
      <dc:date>2017-06-27T17:20:39Z</dc:date>
    </item>
  </channel>
</rss>