<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Real-world SPIFI *write* performance?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Real-world-SPIFI-write-performance/m-p/669177#M26770</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a LPC43xx running at full speed and get SGPIO data in at about 200Mbit/s (25MB/s). I need to store samples for a couple of seconds which requires at least 64 MB, if possible much more, amount of memory for storage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Storing to internal RAM works fine, but it's only about 64-128 kB at most.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All interfaces that require a driver and file system are too slow (USB host, SD card).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;External SDRAM (at 32bit EMC) comes close, but can't quite keep up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So now I'm looking at SPIFI, especially the S25FL512S device. NXP marketing material indicates a 52MB/s bidirectional (read and write) interface to a SPIFI part. I've seen tests that confirm a 40-45 MB/s read performance... &amp;nbsp;but what about writes...?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will any external SPIFI part ever get me a ~25 MB/s write performance? If not, any other ideas how write 64+MB of data at 25 MB/s from a LPC43xx controller?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 07 May 2017 23:27:02 GMT</pubDate>
    <dc:creator>zzzmqp</dc:creator>
    <dc:date>2017-05-07T23:27:02Z</dc:date>
    <item>
      <title>Real-world SPIFI *write* performance?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Real-world-SPIFI-write-performance/m-p/669177#M26770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a LPC43xx running at full speed and get SGPIO data in at about 200Mbit/s (25MB/s). I need to store samples for a couple of seconds which requires at least 64 MB, if possible much more, amount of memory for storage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Storing to internal RAM works fine, but it's only about 64-128 kB at most.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All interfaces that require a driver and file system are too slow (USB host, SD card).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;External SDRAM (at 32bit EMC) comes close, but can't quite keep up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So now I'm looking at SPIFI, especially the S25FL512S device. NXP marketing material indicates a 52MB/s bidirectional (read and write) interface to a SPIFI part. I've seen tests that confirm a 40-45 MB/s read performance... &amp;nbsp;but what about writes...?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will any external SPIFI part ever get me a ~25 MB/s write performance? If not, any other ideas how write 64+MB of data at 25 MB/s from a LPC43xx controller?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 May 2017 23:27:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Real-world-SPIFI-write-performance/m-p/669177#M26770</guid>
      <dc:creator>zzzmqp</dc:creator>
      <dc:date>2017-05-07T23:27:02Z</dc:date>
    </item>
    <item>
      <title>Re: Real-world SPIFI *write* performance?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Real-world-SPIFI-write-performance/m-p/669178#M26771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi zzzmqp,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The write performance will be limited by the program and erase rates of the Flash part, in the case of the S25FL512S device the Programming rate is 1.5 Mbytes/s.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 May 2017 00:04:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Real-world-SPIFI-write-performance/m-p/669178#M26771</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-05-17T00:04:35Z</dc:date>
    </item>
    <item>
      <title>Re: Real-world SPIFI *write* performance?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Real-world-SPIFI-write-performance/m-p/669179#M26772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for confirming, Carlos, that does help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 May 2017 17:02:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Real-world-SPIFI-write-performance/m-p/669179#M26772</guid>
      <dc:creator>zzzmqp</dc:creator>
      <dc:date>2017-05-17T17:02:14Z</dc:date>
    </item>
  </channel>
</rss>