<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックSDIO Errata + SDRAM on LPCXPRESSO 54608 Notice</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDIO-Errata-SDRAM-on-LPCXPRESSO-54608-Notice/m-p/668997#M26755</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wanted to post a bug warning with the current version of the SDK (2.2) for the LPC54608Xpresso board if you want to use the SD card and external SDRAM simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Per the Errata:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/docs/en/errata/ES_LPC546XX.pdf" title="http://www.nxp.com/docs/en/errata/ES_LPC546XX.pdf"&gt;http://www.nxp.com/docs/en/errata/ES_LPC546XX.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Section 3.7 &amp;nbsp;States that SDIO data line D[4] - D[7] need to configured on the mux for proper 4-bit operation. &amp;nbsp; &amp;nbsp;The errata suggests using unbonded IO in the 180 pin BGA package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCU Xpresso SDK (Version 2.2) uses pins that are shared with the EMC interface. &amp;nbsp; &amp;nbsp;If you have the SDRAM enabled and the pin mux setup for EMC, &amp;nbsp; you will get errors when using any of the SD card drivers in the SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The pin mux settings causing the problem are P1_28,P1_29 and P1_30 (EMC_D12,EMC_D13,EMC_D14)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The pin mux settings must be changed to used the unbonded IO as described in the errata:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Enable the SD_D[4] function and on-chip pull-up resistor (via IOCON) on pin PIO4_29.&lt;/P&gt;&lt;P&gt;2. Enable the SD_D[5] function and on-chip pull-up resistor (via IOCON) on pin PIO4_30.&lt;/P&gt;&lt;P&gt;3. Enable the SD_D[6] function and on-chip pull-up resistor (via IOCON) on pin PIO4_31.&lt;/P&gt;&lt;P&gt;4. Enable the SD_D[7] function and on-chip pull-up resistor (via IOCON) on pin PIO5_0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Aug 2017 18:21:36 GMT</pubDate>
    <dc:creator>Eli_H</dc:creator>
    <dc:date>2017-08-07T18:21:36Z</dc:date>
    <item>
      <title>SDIO Errata + SDRAM on LPCXPRESSO 54608 Notice</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDIO-Errata-SDRAM-on-LPCXPRESSO-54608-Notice/m-p/668997#M26755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wanted to post a bug warning with the current version of the SDK (2.2) for the LPC54608Xpresso board if you want to use the SD card and external SDRAM simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Per the Errata:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/docs/en/errata/ES_LPC546XX.pdf" title="http://www.nxp.com/docs/en/errata/ES_LPC546XX.pdf"&gt;http://www.nxp.com/docs/en/errata/ES_LPC546XX.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Section 3.7 &amp;nbsp;States that SDIO data line D[4] - D[7] need to configured on the mux for proper 4-bit operation. &amp;nbsp; &amp;nbsp;The errata suggests using unbonded IO in the 180 pin BGA package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCU Xpresso SDK (Version 2.2) uses pins that are shared with the EMC interface. &amp;nbsp; &amp;nbsp;If you have the SDRAM enabled and the pin mux setup for EMC, &amp;nbsp; you will get errors when using any of the SD card drivers in the SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The pin mux settings causing the problem are P1_28,P1_29 and P1_30 (EMC_D12,EMC_D13,EMC_D14)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The pin mux settings must be changed to used the unbonded IO as described in the errata:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Enable the SD_D[4] function and on-chip pull-up resistor (via IOCON) on pin PIO4_29.&lt;/P&gt;&lt;P&gt;2. Enable the SD_D[5] function and on-chip pull-up resistor (via IOCON) on pin PIO4_30.&lt;/P&gt;&lt;P&gt;3. Enable the SD_D[6] function and on-chip pull-up resistor (via IOCON) on pin PIO4_31.&lt;/P&gt;&lt;P&gt;4. Enable the SD_D[7] function and on-chip pull-up resistor (via IOCON) on pin PIO5_0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Aug 2017 18:21:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDIO-Errata-SDRAM-on-LPCXPRESSO-54608-Notice/m-p/668997#M26755</guid>
      <dc:creator>Eli_H</dc:creator>
      <dc:date>2017-08-07T18:21:36Z</dc:date>
    </item>
  </channel>
</rss>