<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC4357 driver 7inch LCD has blink problem</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-driver-7inch-LCD-has-blink-problem/m-p/666992#M26678</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPC4357 driver 7inch lcd,and running emWin-V5.30.HCLK=204MHz, EMC-SDRAM-MT48LC2M32B2TG-6 and EMC-clock is 102M. Then ,i create a emWin page,and loop&amp;nbsp;call&amp;nbsp;WM_InvalidateWindow() to repaint the page,code such as:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;h_menu = page_system_menu();&lt;BR /&gt; while(1)&lt;BR /&gt; {&lt;BR /&gt; GUI_Delay(1000);&lt;BR /&gt; WM_InvalidateWindow(h_menu);&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;Now ,the problem is that &amp;nbsp;the page is blinking,and i can see the BUTTON on page is cleared and then the BUTTON redraw.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but when i use the emWin Lib-V5.12 to replace the V5.30,the problem is no&amp;nbsp;appear。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 May 2017 09:43:45 GMT</pubDate>
    <dc:creator>skysky</dc:creator>
    <dc:date>2017-05-04T09:43:45Z</dc:date>
    <item>
      <title>LPC4357 driver 7inch LCD has blink problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-driver-7inch-LCD-has-blink-problem/m-p/666992#M26678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPC4357 driver 7inch lcd,and running emWin-V5.30.HCLK=204MHz, EMC-SDRAM-MT48LC2M32B2TG-6 and EMC-clock is 102M. Then ,i create a emWin page,and loop&amp;nbsp;call&amp;nbsp;WM_InvalidateWindow() to repaint the page,code such as:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;h_menu = page_system_menu();&lt;BR /&gt; while(1)&lt;BR /&gt; {&lt;BR /&gt; GUI_Delay(1000);&lt;BR /&gt; WM_InvalidateWindow(h_menu);&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;Now ,the problem is that &amp;nbsp;the page is blinking,and i can see the BUTTON on page is cleared and then the BUTTON redraw.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but when i use the emWin Lib-V5.12 to replace the V5.30,the problem is no&amp;nbsp;appear。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 09:43:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-driver-7inch-LCD-has-blink-problem/m-p/666992#M26678</guid>
      <dc:creator>skysky</dc:creator>
      <dc:date>2017-05-04T09:43:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357 driver 7inch LCD has blink problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-driver-7inch-LCD-has-blink-problem/m-p/666993#M26679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sky Sky,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tested the version 5.38 to see if the same behavior is present?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/webapp/sps/download/license.jsp?colCode=NXP-emWin538-libraries&amp;amp;Parent_nodeId=1460998128877693391064&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/sps/download/license.jsp?colCode=NXP-emWin538-libraries&amp;amp;Parent_nodeId=1460998128877693391064&amp;amp;Parent_pageType=product"&gt;Segger emWin 5.38 Libraries and Utilities for NXP Cortex M3/M4 MCUs&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 23:26:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-driver-7inch-LCD-has-blink-problem/m-p/666993#M26679</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-05-12T23:26:54Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357 driver 7inch LCD has blink problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-driver-7inch-LCD-has-blink-problem/m-p/666994#M26680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello Carlos:&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thank you for your reply.&lt;/P&gt;&lt;P&gt;i have tested the V5.38,the result is the same as V5.30.&lt;/P&gt;&lt;P&gt;In addition,i found the LPC4357's LCD DMA-FIFO don't support 32bit RGB-data.&lt;/P&gt;&lt;P&gt;Then ,when configure the emWin to 24bit RGB,the lcd display is error.&lt;/P&gt;&lt;P&gt;Only configure the emWin to 16bit or 32bit.&lt;/P&gt;&lt;P&gt;but LPC4357 don't support alpha blending,so &amp;nbsp;32bit ARGB is used as 24bit RGB is very bad: no alpha blending,and SDRAM is bigger 50%.&lt;/P&gt;&lt;P&gt;Is this issue exist?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 May 2017 09:56:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-driver-7inch-LCD-has-blink-problem/m-p/666994#M26680</guid>
      <dc:creator>skysky</dc:creator>
      <dc:date>2017-05-15T09:56:11Z</dc:date>
    </item>
  </channel>
</rss>