<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to use BLE with LPC4330? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665315#M26618</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It has been used&amp;nbsp;with Ardunio and my PC successfully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HC05/06 was connected to the Arduino and Plugable Bluetooth dongle was connected to the PC. sending data from PC and receiving it by Arduino, it was okay.&lt;/P&gt;&lt;P&gt;but now, the HC05/06 was connected to the LPC4330 board, I can see the received data on the oscilloscope connected to Bluetooth module's pins but how can I write a code using LPCXpresso to print the received data?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code for the UART1 (TX - GPIO1[6] and RX- GPIO1[7])?&lt;/P&gt;&lt;P&gt;and&amp;nbsp;&lt;/P&gt;&lt;P&gt;The code for printing data?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Nabeel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Jan 2017 13:29:44 GMT</pubDate>
    <dc:creator>nabeelfattah</dc:creator>
    <dc:date>2017-01-09T13:29:44Z</dc:date>
    <item>
      <title>How to use BLE with LPC4330?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665313#M26616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been struggled with using BLE board such as HC05/06 for more than one month.&amp;nbsp;&lt;/P&gt;&lt;P&gt;can some tell me how to use BLE with LPC4330 for receiving data then printing this data on the console &amp;nbsp;in LPCXpresso?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BLE is connected to the UART1. All the examples has been tested and tried different ways but not successful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Jan 2017 10:21:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665313#M26616</guid>
      <dc:creator>nabeelfattah</dc:creator>
      <dc:date>2017-01-07T10:21:49Z</dc:date>
    </item>
    <item>
      <title>Re: How to use BLE with LPC4330?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665314#M26617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nabeel,&lt;/P&gt;&lt;P&gt;Do you mean the HC-05/HC-06 module (see &lt;A class="link-titled" href="https://mcuoneclipse.com/2013/06/19/using-the-hc-06-bluetooth-module/" title="https://mcuoneclipse.com/2013/06/19/using-the-hc-06-bluetooth-module/"&gt;Using the HC-06 Bluetooth Module&lt;/A&gt;)? These modules are classic Bluetooth modules, and *not* BLE modules and incompatible with BLE.&lt;/P&gt;&lt;P&gt;It could be that you are missing to add a pull-up to the Rx line, see &lt;A class="link-titled" href="https://mcuoneclipse.com/2014/03/30/getting-bluetooth-working-with-jy-mcu-bt_board-v1-06/" title="https://mcuoneclipse.com/2014/03/30/getting-bluetooth-working-with-jy-mcu-bt_board-v1-06/"&gt;Getting Bluetooth Working with JY-MCU BT_BOARD V1.06&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Jan 2017 19:05:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665314#M26617</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-01-07T19:05:04Z</dc:date>
    </item>
    <item>
      <title>Re: How to use BLE with LPC4330?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665315#M26618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It has been used&amp;nbsp;with Ardunio and my PC successfully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HC05/06 was connected to the Arduino and Plugable Bluetooth dongle was connected to the PC. sending data from PC and receiving it by Arduino, it was okay.&lt;/P&gt;&lt;P&gt;but now, the HC05/06 was connected to the LPC4330 board, I can see the received data on the oscilloscope connected to Bluetooth module's pins but how can I write a code using LPCXpresso to print the received data?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code for the UART1 (TX - GPIO1[6] and RX- GPIO1[7])?&lt;/P&gt;&lt;P&gt;and&amp;nbsp;&lt;/P&gt;&lt;P&gt;The code for printing data?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Nabeel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jan 2017 13:29:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665315#M26618</guid>
      <dc:creator>nabeelfattah</dc:creator>
      <dc:date>2017-01-09T13:29:44Z</dc:date>
    </item>
    <item>
      <title>Re: How to use BLE with LPC4330?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665316#M26619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To print on the console, use printf()&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See&amp;nbsp;&lt;A href="https://community.nxp.com/message/630895"&gt;https://community.nxp.com/message/630895&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jan 2017 14:54:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665316#M26619</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2017-01-09T14:54:45Z</dc:date>
    </item>
    <item>
      <title>Re: How to use BLE with LPC4330?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665317#M26620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;many thanks Con, what about UART?&lt;/P&gt;&lt;P&gt;What is&amp;nbsp;the input for the printf()?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jan 2017 15:29:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665317#M26620</guid>
      <dc:creator>nabeelfattah</dc:creator>
      <dc:date>2017-01-09T15:29:51Z</dc:date>
    </item>
    <item>
      <title>Re: How to use BLE with LPC4330?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665318#M26621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are lots of UART examples in LPCOpen for the LPC43xx family&lt;/P&gt;&lt;P&gt;printf and scanf both use the console.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jan 2017 15:53:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-BLE-with-LPC4330/m-p/665318#M26621</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2017-01-09T15:53:37Z</dc:date>
    </item>
  </channel>
</rss>