<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Interfacing AT24C16D using I2C</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664294#M26529</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Perhaps something like sending 1 or 2 byte addresses to the I2C device?&lt;/P&gt;&lt;P&gt;The mentioned AT24 device seems to have more than 255 bytes therefore needs two bytes to be sent to address the correct byte in device. But don't mix this address with I2C device address.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 02 Oct 2016 16:15:25 GMT</pubDate>
    <dc:creator>martin_maurer</dc:creator>
    <dc:date>2016-10-02T16:15:25Z</dc:date>
    <item>
      <title>Interfacing AT24C16D using I2C</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664293#M26528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to interface AT24C16D EEPROM through I2C protocol with LPC1549. I am trying to use &lt;A href="https://community.nxp.com/t5/tag/LPCOpen./tg-p"&gt;#LPCOpen.&lt;/A&gt; But, it seems, the LPC Open library for I2C Master is not&amp;nbsp;compatible with&amp;nbsp;#&lt;SPAN&gt;AT24C16D. I guess, it has been tested with LM75 whose addressing is different from AT24C16D. Does anyone have any sample piece of code of interfacing AT24C16D with #LPC1549 using LPC Open library ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Note : When I tried twisting the LPC Open library code to make it work as per the data sheet of AT24C16D it didn't work and I was getting NACK_ADDR from the slave.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Any hint, any sample piece of code (using LPC Open) would be highly appreciable.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Oct 2016 15:56:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664293#M26528</guid>
      <dc:creator>shantanudhar</dc:creator>
      <dc:date>2016-10-02T15:56:37Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing AT24C16D using I2C</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664294#M26529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Perhaps something like sending 1 or 2 byte addresses to the I2C device?&lt;/P&gt;&lt;P&gt;The mentioned AT24 device seems to have more than 255 bytes therefore needs two bytes to be sent to address the correct byte in device. But don't mix this address with I2C device address.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Oct 2016 16:15:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664294#M26529</guid>
      <dc:creator>martin_maurer</dc:creator>
      <dc:date>2016-10-02T16:15:25Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing AT24C16D using I2C</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664295#M26530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;You got it right. Yes AT24C16D EEPROM has 2 bytes addressing mechanism. 1st byte defines the 4bit device ID which is fixed, 3 bit page ID and R/W bit. The next byte is the 8 bit address in the mentioned page ID. So, as mentioned in the spec, I wss sending the START bit first and then the 1st address byte and then 2nd. But, after the 1st address byte I am receiving NACK_ADR from the slave. I am wandering what wrong I did.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Oct 2016 16:39:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664295#M26530</guid>
      <dc:creator>shantanudhar</dc:creator>
      <dc:date>2016-10-02T16:39:01Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing AT24C16D using I2C</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664296#M26531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the below link, this may helps &lt;A class="link-titled" href="https://fjrg76.wordpress.com/2014/12/11/reading-and-writing-a-24lc32a-eeprom-memory-using-the-lpcopen-framework-for-the-lpc1549-chip/" title="https://fjrg76.wordpress.com/2014/12/11/reading-and-writing-a-24lc32a-eeprom-memory-using-the-lpcopen-framework-for-the-lpc1549-chip/"&gt;Reading and writing a 24LC32A eeprom memory using the LPCOpen framework for the LPC1549 chip | Sistemas embebidos en esp…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 21:09:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664296#M26531</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-10-07T21:09:46Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing AT24C16D using I2C</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664297#M26532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks @soledad. I will try this link. But, I guess, the implementation in&amp;nbsp;LPC Open differs in the following section:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is an excerpt from the AT24C16D data sheet (&lt;A class="link-titled" href="http://www.atmel.com/images/Atmel-8906-SEEPROM-AT24C16D-Datasheet.pdf" title="http://www.atmel.com/images/Atmel-8906-SEEPROM-AT24C16D-Datasheet.pdf"&gt;http://www.atmel.com/images/Atmel-8906-SEEPROM-AT24C16D-Datasheet.pdf&lt;/A&gt;&amp;nbsp;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;5 Write Operations&lt;/P&gt;&lt;P&gt;All Write operations for the AT24C16D begin with the Master sending a Start condition, followed by a Device Address byte with the R/W bit set to ‘0’, and then by the Word Address byte. The data value(s) to be written to the device immediately follow the Word Address byte.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But, the way LPC Open handles a write operation is different and follows&amp;nbsp;the datasheet of LM75 temperature sensor. So, I am in doubt if I can at all use LPC Open for handling AT24C16D.‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anybody from the lpc1549‌ team help me to confirm&amp;nbsp;if lpcopen&amp;nbsp;v2.20 is compatible with AT24C16D eeprom ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Oct 2016 11:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664297#M26532</guid>
      <dc:creator>shantanudhar</dc:creator>
      <dc:date>2016-10-19T11:31:33Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing AT24C16D using I2C</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664298#M26533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is working. Thanks Sol&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Oct 2016 23:27:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Interfacing-AT24C16D-using-I2C/m-p/664298#M26533</guid>
      <dc:creator>shantanudhar</dc:creator>
      <dc:date>2016-10-19T23:27:40Z</dc:date>
    </item>
  </channel>
</rss>