<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC17xx ClkOut function as system clock in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-ClkOut-function-as-system-clock/m-p/518387#M2643</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdurand on Wed Aug 08 13:57:17 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've used CLKOUT on other processors to run other chips, but note that a 48MHz signal doesn't like to travel very far unless it's buffered and terminated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It's not THAT high, but it's fast enough I'd worry about running more than one or two other chips and they should be physically close.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:33:15 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:33:15Z</dc:date>
    <item>
      <title>LPC17xx ClkOut function as system clock</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-ClkOut-function-as-system-clock/m-p/518386#M2642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tech19 on Wed Aug 08 00:06:42 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In LPC17xx User manual (Section 4.10) it has been stated that :&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"For system test and development purposes, any one of several internal clocks may be&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;brought out on the CLKOUT function available on the P1.27 pin, as shown in Figure 12."&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there any problem if the CLKOUT function remains permanently ON to feed other parts as system clock ? I mean why manual has emphasized&amp;nbsp; "For system test and development purposes" ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Should I reconsider using CLKOUT @48MHZ as system clock ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sincerely,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Tech19&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-ClkOut-function-as-system-clock/m-p/518386#M2642</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC17xx ClkOut function as system clock</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-ClkOut-function-as-system-clock/m-p/518387#M2643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdurand on Wed Aug 08 13:57:17 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've used CLKOUT on other processors to run other chips, but note that a 48MHz signal doesn't like to travel very far unless it's buffered and terminated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It's not THAT high, but it's fast enough I'd worry about running more than one or two other chips and they should be physically close.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:33:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-ClkOut-function-as-system-clock/m-p/518387#M2643</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:33:15Z</dc:date>
    </item>
    <item>
      <title>Re: LPC17xx ClkOut function as system clock</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-ClkOut-function-as-system-clock/m-p/518388#M2644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tech19 on Thu Aug 09 23:20:34 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the feedback.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can take care of the layout issues if I can use it. Actually I want to feed it to a CPLD which in turn will feed other components. The main issue is that I want a Sync clock with LPC. It is very convenient if I can use CLKOUT function as CPLD clock. My main worry is that maybe turning this function On may introduce unspecified problems.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:33:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-ClkOut-function-as-system-clock/m-p/518388#M2644</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:33:16Z</dc:date>
    </item>
  </channel>
</rss>