<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Driving LPC2131 VDD above the Absolute Maximum Rating</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Driving-LPC2131-VDD-above-the-Absolute-Maximum-Rating/m-p/662563#M26418</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have been using the LPC2131 in our design for years and driving it (VDD) at 3.3V. We just realized that our board voltage monitoring circuit would not triggered an error until the voltage goes above 3.9V for VDD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As&amp;nbsp;of safety concern, what would happen to the device if it would be feed at 3.9V instead of 3.3V ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would it catch into fire or it would only reduce its MTBF and affect its behavior/performance&amp;nbsp;?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2017 19:36:06 GMT</pubDate>
    <dc:creator>sylvainpoulin</dc:creator>
    <dc:date>2017-02-22T19:36:06Z</dc:date>
    <item>
      <title>Driving LPC2131 VDD above the Absolute Maximum Rating</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Driving-LPC2131-VDD-above-the-Absolute-Maximum-Rating/m-p/662563#M26418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have been using the LPC2131 in our design for years and driving it (VDD) at 3.3V. We just realized that our board voltage monitoring circuit would not triggered an error until the voltage goes above 3.9V for VDD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As&amp;nbsp;of safety concern, what would happen to the device if it would be feed at 3.9V instead of 3.3V ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would it catch into fire or it would only reduce its MTBF and affect its behavior/performance&amp;nbsp;?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 19:36:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Driving-LPC2131-VDD-above-the-Absolute-Maximum-Rating/m-p/662563#M26418</guid>
      <dc:creator>sylvainpoulin</dc:creator>
      <dc:date>2017-02-22T19:36:06Z</dc:date>
    </item>
    <item>
      <title>Re: Driving LPC2131 VDD above the Absolute Maximum Rating</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Driving-LPC2131-VDD-above-the-Absolute-Maximum-Rating/m-p/662564#M26419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. Would it catch into fire or it would only reduce its MTBF?&lt;/P&gt;&lt;P&gt;A. There is no definite answer to this question. Both cases are possible.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2017 09:57:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Driving-LPC2131-VDD-above-the-Absolute-Maximum-Rating/m-p/662564#M26419</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-02-28T09:57:19Z</dc:date>
    </item>
  </channel>
</rss>