<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC-Link + LabTool with external RAM and data streaming via Wi-Fi in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-LabTool-with-external-RAM-and-data-streaming-via-Wi-Fi/m-p/660871#M26282</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="228832" data-username="hmyoong" href="https://community.nxp.com/people/hmyoong"&gt;HM Yoong&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;/P&gt;&lt;P&gt;In my opinion, I don't think the LabTool can achieve the implementation, as the LabTtool hasn't provide the UART interface to connect the WiFi module likes the ESP8266.&lt;/P&gt;&lt;P&gt;And it's not necessary to add an external SDRAM when sampled data is transferred to WiFI module periodically.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Feb 2017 05:57:58 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2017-02-24T05:57:58Z</dc:date>
    <item>
      <title>LPC-Link + LabTool with external RAM and data streaming via Wi-Fi</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-LabTool-with-external-RAM-and-data-streaming-via-Wi-Fi/m-p/660870#M26281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to use LPC-Link2 and LabTool to sample analog data up to 80 Msps for 0.1 and transfer the data remotely via ESP8266 or other Wi-Fi transceiver. &amp;nbsp;LPC4370 only has 282 kB RAM. &amp;nbsp;Doing the maths and with the non-deterministic nature of TCP/IP, is there a better to do it? I do not have the expertise and time to develop my own boards with external SDRAM and required hardware from LabTool. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 15:46:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-LabTool-with-external-RAM-and-data-streaming-via-Wi-Fi/m-p/660870#M26281</guid>
      <dc:creator>hmyoong</dc:creator>
      <dc:date>2017-02-22T15:46:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link + LabTool with external RAM and data streaming via Wi-Fi</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-LabTool-with-external-RAM-and-data-streaming-via-Wi-Fi/m-p/660871#M26282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="228832" data-username="hmyoong" href="https://community.nxp.com/people/hmyoong"&gt;HM Yoong&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;/P&gt;&lt;P&gt;In my opinion, I don't think the LabTool can achieve the implementation, as the LabTtool hasn't provide the UART interface to connect the WiFi module likes the ESP8266.&lt;/P&gt;&lt;P&gt;And it's not necessary to add an external SDRAM when sampled data is transferred to WiFI module periodically.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Feb 2017 05:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-LabTool-with-external-RAM-and-data-streaming-via-Wi-Fi/m-p/660871#M26282</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2017-02-24T05:57:58Z</dc:date>
    </item>
  </channel>
</rss>