<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Is the LPC4337JET256 compatible with the LPC1837JET256</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-the-LPC4337JET256-compatible-with-the-LPC1837JET256/m-p/660293#M26229</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="288086" data-username="tonyvinto" href="https://community.nxp.com/people/tonyvinto"&gt;Tony Vinto&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Can I drop this Cortex M4 onto my board in place of the Cortex M3 part and expect it to work?&lt;/P&gt;&lt;P&gt;Yes, and LPC1800's pin assignment is compatible with the LPC4300.&lt;/P&gt;&lt;P&gt;The bug is also exist in the initial device revision of the LPC4337, but not in the second revision.&lt;/P&gt;&lt;P&gt;Hope this is clear.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Dec 2016 02:24:29 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-12-14T02:24:29Z</dc:date>
    <item>
      <title>Is the LPC4337JET256 compatible with the LPC1837JET256</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-the-LPC4337JET256-compatible-with-the-LPC1837JET256/m-p/660292#M26228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can I drop this Cortex M4 onto my board in place of the Cortex M3 part and expect it to work? &amp;nbsp;The datasheet makes em loop awfully compatible but it does not come out and say it is. &amp;nbsp;I want to make use of the extra clock speed and the math co-processor. &amp;nbsp;So I would only expect to modify initialization code for the 204MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any gotchas that I need to know about. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What about eratta? &amp;nbsp;The 1837 had that CAN problem in rev "-". &amp;nbsp;Has the rev A of the 4337 been released with that fix?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2016 17:07:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-the-LPC4337JET256-compatible-with-the-LPC1837JET256/m-p/660292#M26228</guid>
      <dc:creator>tonyvinto</dc:creator>
      <dc:date>2016-12-08T17:07:48Z</dc:date>
    </item>
    <item>
      <title>Re: Is the LPC4337JET256 compatible with the LPC1837JET256</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-the-LPC4337JET256-compatible-with-the-LPC1837JET256/m-p/660293#M26229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="288086" data-username="tonyvinto" href="https://community.nxp.com/people/tonyvinto"&gt;Tony Vinto&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Can I drop this Cortex M4 onto my board in place of the Cortex M3 part and expect it to work?&lt;/P&gt;&lt;P&gt;Yes, and LPC1800's pin assignment is compatible with the LPC4300.&lt;/P&gt;&lt;P&gt;The bug is also exist in the initial device revision of the LPC4337, but not in the second revision.&lt;/P&gt;&lt;P&gt;Hope this is clear.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 02:24:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-the-LPC4337JET256-compatible-with-the-LPC1837JET256/m-p/660293#M26229</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-12-14T02:24:29Z</dc:date>
    </item>
  </channel>
</rss>