<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1679CMSIS BOARD - I2C example - finding slave devices</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1679CMSIS-BOARD-I2C-example-finding-slave-devices/m-p/654347#M26009</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomasz XYZ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I think you are talking the LPC1769, not the LPC1679.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please tell me where you download the code which you are using, I can't find the source, please give me link, I will help you to check it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Actually, about the device address, normally, it is defined in the I2C initialization code, if you can't find it from the code. Please tell me your code download link, I will help you to check it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Waiting for your reply!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Apr 2017 08:18:09 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2017-04-12T08:18:09Z</dc:date>
    <item>
      <title>LPC1679CMSIS BOARD - I2C example - finding slave devices</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1679CMSIS-BOARD-I2C-example-finding-slave-devices/m-p/654346#M26008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just started with LPC. So sorry for newie questions...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to connect LCD 16x2 via I2C (PCF85741 - mounted on LCD &lt;SPAN style="color: #1155cc; text-decoration: underline; font-size: 10.0pt; font-family: 'Arial',sans-serif;"&gt;&lt;A href="https://botland.com.pl/wyswietlacze-alfanumeryczne/2351-wyswietlacz-lcd-2x16-znakow-niebieski-konwerter-i2c-lcm1602.html" target="_blank"&gt;https://botland.com.pl/wyswietlacze-alfanumeryczne/2351-wyswietlacz-lcd-2x16-znakow-niebieski-konwerter-i2c-lcm1602.html&lt;/A&gt;&lt;/SPAN&gt;). I'm not sure about adress of this device and i wanted to use demo "periph_i2c" to findout it (option 3 in i2cmenu via UART). So that is my questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- There are two options (Select I2C peripheral). At I2C0 are virtual devices. I2C1 is exacly whith pins? (I connected device into P0.10 and P0.11). I just want to know device adress. After connect devices program just do it and not responding :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Select an option [0 - 6] :ý˙˙ţý˙**************** I2C Demo Menu ****************&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;0: Exit Demo&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;1: Select I2C peripheral [[1B][1;32mI2C0[1B][0;37m]&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;2: Toggle mode POLLING/INTERRUPT [[1B][1;32mINTERRUPT[1B][0;37m]&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;3: Probe for Slave devices&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;4: Read slave data&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;5: Write slave data&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;6: Write/Read slave data&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Select an option [0 - 6] :1&lt;BR /&gt;1&lt;BR /&gt;Select I2C device [0 or 1] : 1&lt;BR /&gt;1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;**************** I2C Demo Menu ****************&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;0: Exit Demo&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;1: Select I2C peripheral [[1B][1;32mI2C1[1B][0;37m]&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;2: Toggle mode POLLING/INTERRUPT [[1B][1;32mINTERRUPT[1B][0;37m]&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;3: Probe for Slave devices&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;4: Read slave data&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;5: Write slave data&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;6: Write/Read slave data&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Select an option [0 - 6] :3&lt;BR /&gt;3&lt;BR /&gt;Probing available I2C devices...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00 01 02 03 04 05 06 07 08 09 0A 0B 0C 0D 0E 0F&lt;BR /&gt;====================================================&lt;BR /&gt;00&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Apr 2017 13:08:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1679CMSIS-BOARD-I2C-example-finding-slave-devices/m-p/654346#M26008</guid>
      <dc:creator>tomaszxyz</dc:creator>
      <dc:date>2017-04-06T13:08:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1679CMSIS BOARD - I2C example - finding slave devices</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1679CMSIS-BOARD-I2C-example-finding-slave-devices/m-p/654347#M26009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomasz XYZ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I think you are talking the LPC1769, not the LPC1679.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please tell me where you download the code which you are using, I can't find the source, please give me link, I will help you to check it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Actually, about the device address, normally, it is defined in the I2C initialization code, if you can't find it from the code. Please tell me your code download link, I will help you to check it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Waiting for your reply!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2017 08:18:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1679CMSIS-BOARD-I2C-example-finding-slave-devices/m-p/654347#M26009</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-04-12T08:18:09Z</dc:date>
    </item>
  </channel>
</rss>