<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックUsing LPCOpen in keil with KEIL USB library</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPCOpen-in-keil-with-KEIL-USB-library/m-p/653889#M25982</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using lpc1788 and KEIL 5.2.2. I want to use LPCOpen drivers in keil and also use KEIL USB library (and other libraries such as graphics library).&lt;/P&gt;&lt;P&gt;I have problem in the project because of LPCOpen conflicts with keil cmsis header (LPC17X_8X.h) and startup file (system_LPC177x_8x.h).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does any body use LPCOpen in Keil with keil package libraries?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(Sorry for my bad english)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Dec 2016 11:17:44 GMT</pubDate>
    <dc:creator>dolphinapadana</dc:creator>
    <dc:date>2016-12-07T11:17:44Z</dc:date>
    <item>
      <title>Using LPCOpen in keil with KEIL USB library</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPCOpen-in-keil-with-KEIL-USB-library/m-p/653889#M25982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using lpc1788 and KEIL 5.2.2. I want to use LPCOpen drivers in keil and also use KEIL USB library (and other libraries such as graphics library).&lt;/P&gt;&lt;P&gt;I have problem in the project because of LPCOpen conflicts with keil cmsis header (LPC17X_8X.h) and startup file (system_LPC177x_8x.h).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does any body use LPCOpen in Keil with keil package libraries?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(Sorry for my bad english)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Dec 2016 11:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPCOpen-in-keil-with-KEIL-USB-library/m-p/653889#M25982</guid>
      <dc:creator>dolphinapadana</dc:creator>
      <dc:date>2016-12-07T11:17:44Z</dc:date>
    </item>
    <item>
      <title>Re: Using LPCOpen in keil with KEIL USB library</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPCOpen-in-keil-with-KEIL-USB-library/m-p/653890#M25983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="291246" data-username="dolphinapadana" href="https://community.nxp.com/people/dolphinapadana"&gt;Dolphin Apadana&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;The LPC177x and LPC178x CMSIS-Compliant standard peripheral firmware driver library is the choice if you want to the KEIL USB library.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.lpcware.com/content/nxpfile/lpc177x-and-lpc178x-cmsis-compliant-standard-peripheral-firmware-driver-library-keil" title="https://www.lpcware.com/content/nxpfile/lpc177x-and-lpc178x-cmsis-compliant-standard-peripheral-firmware-driver-library-keil"&gt;LPC177x and LPC178x CMSIS-Compliant Standard Peripheral Firmware Driver Library (Keil, IAR) | www.LPCware.com&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 03:04:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPCOpen-in-keil-with-KEIL-USB-library/m-p/653890#M25983</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-12-09T03:04:42Z</dc:date>
    </item>
    <item>
      <title>Re: Using LPCOpen in keil with KEIL USB library</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPCOpen-in-keil-with-KEIL-USB-library/m-p/653891#M25984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Tank you for your answer.&lt;/P&gt;&lt;P&gt;Because i want to migrate to LPC4357 MCU and because of optimizations in LPCOpen (I like the inline functions) i decide to use LPCOpen.&lt;/P&gt;&lt;P&gt;I use a workaround for my project, I replace all the conflicts of CMSIS library in LPCOpen. for example i replace LPC_GPIO to CHIP_LPC_GPIO&lt;/P&gt;&lt;P&gt;so from this time i use CHIP_LPC_XXX keyword in my code.&lt;/P&gt;&lt;P&gt;The only bad thing is that i should do this work for all the other LPCOpen libraries i will use in future (Like LPC43XX).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Dec 2016 06:50:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPCOpen-in-keil-with-KEIL-USB-library/m-p/653891#M25984</guid>
      <dc:creator>dolphinapadana</dc:creator>
      <dc:date>2016-12-11T06:50:22Z</dc:date>
    </item>
  </channel>
</rss>