<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1114FHN33/302, 1 power consumption and programming in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FHN33-302-1-power-consumption-and-programming/m-p/652594#M25928</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;OL&gt;&lt;LI&gt;What is the typical power consumption for this processor during flash erase&amp;nbsp; and program cycles. We are using ISP/bootrom reprograming.&lt;/LI&gt;&lt;LI style="color: #000000; font-size: 11pt;"&gt;For&amp;nbsp; &amp;nbsp;IOCONFIG block (0x40044000) can it be accessed through the ISP “Write to RAM” command.&amp;nbsp; We would like to change the pull-up on pio1_5 to a pull down during programming, but the pin uses its default configuration(input/pull-up) when we reset the processor to enter ISP mode.&lt;/LI&gt;&lt;/OL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Jan 2017 20:07:12 GMT</pubDate>
    <dc:creator>PaulJoseph</dc:creator>
    <dc:date>2017-01-27T20:07:12Z</dc:date>
    <item>
      <title>LPC1114FHN33/302, 1 power consumption and programming</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FHN33-302-1-power-consumption-and-programming/m-p/652594#M25928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;OL&gt;&lt;LI&gt;What is the typical power consumption for this processor during flash erase&amp;nbsp; and program cycles. We are using ISP/bootrom reprograming.&lt;/LI&gt;&lt;LI style="color: #000000; font-size: 11pt;"&gt;For&amp;nbsp; &amp;nbsp;IOCONFIG block (0x40044000) can it be accessed through the ISP “Write to RAM” command.&amp;nbsp; We would like to change the pull-up on pio1_5 to a pull down during programming, but the pin uses its default configuration(input/pull-up) when we reset the processor to enter ISP mode.&lt;/LI&gt;&lt;/OL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2017 20:07:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FHN33-302-1-power-consumption-and-programming/m-p/652594#M25928</guid>
      <dc:creator>PaulJoseph</dc:creator>
      <dc:date>2017-01-27T20:07:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1114FHN33/302, 1 power consumption and programming</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FHN33-302-1-power-consumption-and-programming/m-p/652595#M25929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.- When I perform an IAP erase and program of all sectors at 12 MHz I measure a total device current of 3.20 mA (3.3 v). I don’t expect the total current to vary a lot from the datasheet typical numbers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.- It can't be accessed, if you attempt to write an address other than RAM using the "Write to RAM" command you will receive a SRC_ADDR_NOT_MAPPED return code.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 00:06:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FHN33-302-1-power-consumption-and-programming/m-p/652595#M25929</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2017-02-03T00:06:15Z</dc:date>
    </item>
  </channel>
</rss>