<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Lpc 824 DMA to GPIO</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc-824-DMA-to-GPIO/m-p/650906#M25876</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, it was a couple of years now, but for 824 it can't use DMA to access gpio, i was always getting dma erros.&lt;/P&gt;&lt;P&gt;And reason is that GPIO is "tightly" coupled to core.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If your LPC has same architecture as on picture above, than i think it can not work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But if GPIO is connected to AHB bus and DMA is connected to it it might work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does that uC has DMA?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR/Tvrtko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Apr 2020 08:06:42 GMT</pubDate>
    <dc:creator>tvrklejelani</dc:creator>
    <dc:date>2020-04-21T08:06:42Z</dc:date>
    <item>
      <title>Lpc 824 DMA to GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc-824-DMA-to-GPIO/m-p/650903#M25873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i have problems driving lpc gpio port using dma. When i write with dma to any ram adress everything &amp;nbsp;works fine, but when i write to any of registers associated with gpio nothing happens.&lt;/P&gt;&lt;P&gt;My question is... Can 824 use dma to write to gpio.&lt;/P&gt;&lt;P&gt;Based on block diagram of 824, GPIO is connected to ARM M0+ but not to AHB..is this true?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Dec 2016 13:19:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc-824-DMA-to-GPIO/m-p/650903#M25873</guid>
      <dc:creator>tvrklejelani</dc:creator>
      <dc:date>2016-12-05T13:19:29Z</dc:date>
    </item>
    <item>
      <title>Re: Lpc 824 DMA to GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc-824-DMA-to-GPIO/m-p/650904#M25874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="291521" data-username="tvrklejelani" href="https://community.nxp.com/people/tvrklejelani"&gt;Tvrkle JElani&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.&lt;/P&gt;&lt;P&gt;In my opinion, the GPIO is connected to the APB bus, and it can work with the DMA engine.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 01:23:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc-824-DMA-to-GPIO/m-p/650904#M25874</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-12-09T01:23:51Z</dc:date>
    </item>
    <item>
      <title>Re: Lpc 824 DMA to GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc-824-DMA-to-GPIO/m-p/650905#M25875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you finally find a solution? I'm having the same problem with a LPC11&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2020 12:08:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc-824-DMA-to-GPIO/m-p/650905#M25875</guid>
      <dc:creator>javiervallori</dc:creator>
      <dc:date>2020-04-20T12:08:11Z</dc:date>
    </item>
    <item>
      <title>Re: Lpc 824 DMA to GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc-824-DMA-to-GPIO/m-p/650906#M25876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, it was a couple of years now, but for 824 it can't use DMA to access gpio, i was always getting dma erros.&lt;/P&gt;&lt;P&gt;And reason is that GPIO is "tightly" coupled to core.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If your LPC has same architecture as on picture above, than i think it can not work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But if GPIO is connected to AHB bus and DMA is connected to it it might work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does that uC has DMA?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR/Tvrtko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2020 08:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc-824-DMA-to-GPIO/m-p/650906#M25876</guid>
      <dc:creator>tvrklejelani</dc:creator>
      <dc:date>2020-04-21T08:06:42Z</dc:date>
    </item>
    <item>
      <title>Re: Lpc 824 DMA to GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc-824-DMA-to-GPIO/m-p/650907#M25877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you! the uC has a DMA, and the GPIO seems to be connect to the AHB. But for some reason, setting DMA destination address to the GPIO has no effect.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2020 09:06:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc-824-DMA-to-GPIO/m-p/650907#M25877</guid>
      <dc:creator>javiervallori</dc:creator>
      <dc:date>2020-04-22T09:06:32Z</dc:date>
    </item>
  </channel>
</rss>